| Keysight.Visa Namespace : VxiBackplaneSession Class |
For a list of all members of this type, see VxiBackplaneSession members.
| Name | Description | |
|---|---|---|
![]() | AssertInterrupt | Keysight VISA.NET does not support this method. |
![]() | AssertTrigger | Asserts a software or hardware trigger. |
![]() | AssertUtilitySignal | Keysight VISA.NET does not support this method. |
![]() | DisableEvent | Disables a calling program's ability to receive events of the type specified by the eventType argument using a VisaSession.WaitOnEvent method (any overload). (Inherited from Keysight.Visa.VisaSession) |
![]() | DiscardEvents | Discards events of the type specified by the eventType argument from the queue for that event type. (Inherited from Keysight.Visa.VisaSession) |
![]() | Dispose | Overloaded. Performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this session. (Inherited from Keysight.Visa.VisaSession) |
![]() | EnableEvent | Enables a calling program's ability to receive events of the type specified by the eventType argument using a WaitOnEvent method. (Inherited from Keysight.Visa.VisaSession) |
![]() | LockResource | Overloaded. Acquires a lock on the resource for this session. (Inherited from Keysight.Visa.VisaSession) |
![]() | MapTrigger | Overloaded. Maps the specified source trigger line to the specified destination trigger line. |
![]() | UnlockResource | Unlocks the resource. (Inherited from Keysight.Visa.VisaSession) |
![]() | UnmapTrigger | Overloaded. Unmap the specified source trigger line. |
![]() | WaitOnEvent | Overloaded. Waits for an occurrence of the specified event for this session. In particular, WaitOnEvent suspends execution of the thread on which it is called and waits for the specified event indefinitely. (Inherited from Keysight.Visa.VisaSession) |
| Name | Description | |
|---|---|---|
![]() | Finalize | Performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this session. (Inherited from Keysight.Visa.VisaSession) |