Keysight VISA.NET Help
TriggerStatus Property (VxiBackplaneSession)



The VXI trigger line(s) that are currently set.
Syntax
'Declaration
 
Public ReadOnly Property TriggerStatus As TriggerLines
'Usage
 
Dim instance As VxiBackplaneSession
Dim value As TriggerLines
 
value = instance.TriggerStatus
public TriggerLines TriggerStatus {get;}
public:
property TriggerLines TriggerStatus {
   TriggerLines get();
}
Remarks

All of the members defined in the Ivi.Visa.TriggerLines enumeration are valid for VXI.

TriggerLines has the [Flags] attribute - multiple trigger lines may be specified by OR-ing them together.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025