Keysight VISA.NET Help
DestinationAccessPrivilege Property (VxiSession)



[Register-Based] The address modifier used in high-level access methods, such as OutXX() and MoveOutXX(), when writing to the destination.
Syntax
'Declaration
 
Public Property DestinationAccessPrivilege As VxiAccessPrivilege
'Usage
 
Dim instance As VxiSession
Dim value As VxiAccessPrivilege
 
instance.DestinationAccessPrivilege = value
 
value = instance.DestinationAccessPrivilege
public VxiAccessPrivilege DestinationAccessPrivilege {get; set;}
public:
property VxiAccessPrivilege DestinationAccessPrivilege {
   VxiAccessPrivilege get();
   void set (    VxiAccessPrivilege value);
}
Remarks

The default is DataPrivileged.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025