viAssertUtilSignal
Syntax
viAssertUtilSignal(ViSession vi, ViUInt16 line);
Description
Asserts the specified utility bus signal. This operation can be used to assert either the SYSFAIL or SYSRESET utility bus interrupts on the VXIbus backplane. This operation is valid only on VXI Mainframe Backplane (BACKPLANE) and on Servant Device-Side (SERVANT) resource sessions.
![]() |
This function is not supported in Keysight VISA. You should assert SYSRESET (also known as HARD RESET in the VXI specification) only when it is necessary to promptly terminate operation of all devices in a VXIbus system. This is a serious action that always affects the entire VXIbus system. |
Parameters
Name |
Dir |
Type |
Description |
---|---|---|---|
vi |
IN |
ViSession |
Unique logical identifier to a session. |
line |
IN |
ViUInt16 |
Specifies the utility bus signal to assert. This can be: VI_UTIL_ASSERT_SYSRESET, VI_UTIL_ASSERT_SYSFAIL, or VI_UTIL_DEASSERT_SYSFAIL |
Return Values
Type ViStatus |
This is the function return status. It returns either a completion code or an error code as follows. |
Completion Code |
Description |
---|---|
VI_SUCCESS |
The specified utility bus signal was successfully asserted to the device. |
Error Code |
Description |
VI_ERROR_INV_LINE |
The value specified by the line parameter is invalid. |
VI_ERROR_INV_SESSION |
The given session or object reference is invalid (both are the same value). |
VI_ERROR_NSUP_OPER |
The given vi does not support this function. |
VI_ERROR_RSRC_LOCKED |
Specified operation could not be performed because the resource identified by vi has been locked for this kind of access. |
VI_ERROR_TMO |
Timeout expired before function completed. |
VI_SUCCESS |
Operation completed successfully. |
See Also
BACKPLANE resource description