Getting Started
Install, Uninstall or Update IO Libraries Suite
Refer to the readme.htm file, which is available at the following locations:
-
Navigate to the IO Libraries suite page, under the Trials and Licenses tab, select either the Windows or the Linux readme.
-
From IO Control > Documentation > IO Libraries Suite Readme.
Click to learn how to launch IO Control
With IO Libraries 2025 or later, IO Control is available as a web application. You can launch it in any of the following ways:
From the Application Finder:
-
Open the Application Finder on your Linux machine.
-
Search for IO Control and click to launch it.
Using a Web Browser:
-
Open your preferred web browser.
-
Enter the URL, https://localhost:4214.
-
Launching Connection Expert
There are two methods to launch Connection Expert (CE):
-
From the Application Finder:
-
Open the Application Finder on your Linux machine.
-
Search for Connection Expert under the application section..
-
Click to launch the application.
-
-
Using a Web Browser:
-
Open your preferred web browser.
-
Enter the URL in the format: https://<IP Address of the machine where IO Libraries Suite is installed>:4211.
-
For example: https://10.17.68.235:4211.
-
|
|
Secure Access and Certificate Configuration
To access Connection Expert over a secure HTTPS connection, a trusted certificate must be configured. You can either use the default self-signed certificate or create a locally trusted certificate.
Default Self-Signed Certificate
If a locally trusted certificate is not configured, Connection Expert automatically generates a self-signed certificate for HTTPS. When accessing Interactive IO for the first time from a client machine, your web browser will display a security warning.
To proceed:
-
Click the Advanced button on the warning page.
-
Select Proceed to [IP Address] to open Interactive IO.
Even after accepting the certificate, the browser may continue displaying a warning symbol in the address bar. However, the connection remains secure.
If this is not acceptable for your environment, installing a locally trusted certificate will eliminate the warning.
|
Ensure that your web browser allows self-signed certificates or is configured to trust locally installed certificates to prevent security warnings. |