LAN Interface

A LAN (TCP/IP) interface is a logical collection of properties that can apply to remote interfaces and instruments. A LAN interface does not directly represent physical devices. Several physical devices may be auto-discovered or manually added on a single LAN interface. In this case, the interface properties apply to all related devices.

The default LAN interface is TCPIP0. Changing properties of this interface (such as timeouts) will apply to all its associated LAN instruments. To maintain two or more groups of instruments with different interface properties, add a new LAN interface, and then add instruments specifying the interface whose properties you wish to apply to that instrument.

Adding new interfaces offers several advantages, including enhanced organization of instruments within the view, the ability to utilize various protocols, and greater control over timeout values.

LAN Interface Properties

Click here to learn about LAN interface settings.

Different Types of LAN Connections

 

Related topics: