IO Libraries Suite Updates
In this screen, you'll see the currently-installed version number of the IO Libraries Suite and enables you set future update preference.
By default, if you start Connection Expert and a newer version is available, you will see this screen before being directed to Instruments View as usual.
Setting | Description |
---|---|
Download New Version | If there is a newer version available, you'll see that information and you will have the option to click Download New Version. |
Do Not Suggest Future Updates | To disable this feature, select Do Not Suggest Future Updates, then click OK to save. You can always use the Settings dialog or Keysight.com to view and download available updates. |
To access the readme file for your operating system and other detailed information about available updates to IO Libraries Suite, go to http://www.keysight.com/find/iosuite. The Trials and Licenses tab contains readme links and downloads for both Windows and Linux.