Connection Expert
Connection Expert is a utility in the Keysight IO Libraries Suite that simplifies connecting to instruments on a PC running the suite. It supports a wide range of hardware communication interfaces, including GPIB, USB, Serial, LAN/Ethernet, PXI, and VXI.
Leveraging IO Libraries' discovery capabilities, Connection Expert provides a detailed view of available interfaces and their connected instruments. It allows you to configure connections, monitor real-time connection status, test connectivity, and communicate directly with instruments using command execution.