Getting Started

Install, Uninstall or Update IO Libraries Suite

Connection Expert utilty is available as a part of IO Libraries suite. To install, update or uninstall IO Libraries suite, refer to readme.htm file, which is available at the following locations:

  • Navigate to the IO Libraries suite page, under the Trials and Licenses tab, select either the Windows or the Linux readme.
  • Alternatively, after installing IO Libraries Suite, you can open Readme from IO Control > Documentation > IO Libraries Suite Readme.

Launching Connection Expert

There are two methods to launch Connection Expert (CE):

  • Launch from Desktop:

    • Navigate to your Windows desktop.
    • Locate Keysight Connection Expert and double click it to open.

  • Launch from Start Menu

    • Press Windows Key on your keyboard or click the Start menu.

    • Locate Keysight Connection Expert in the list and click to open it.


Related Topics