PXI/AXIe Chassis

The Chassis View displays a list of chassis connected to the selected test stations.

NOTE
  • A test station is a PC with IO Libraries Suite, used to discover, track, and monitor devices.

# Description
1

Show Chassis PCIe Connection Hierarchy -Toggles between hierarchical and flat views of chassis connectivity. The hierarchical view illustrates how a chassis connects—either directly to the system or through another chassis.

2

Chassis Content - Displays the chassis details.

3 Chassis Triggers - Shows reserved trigger lines and routes. Lets you reserve/unreserve lines and add/remove routes.
4 Chassis Numbers - Displays available chassis numbers and lets you reassign them as needed