Interface IUsb
Description
The IUsb interface defines the methods and COM properties specific to USB INSTR sessions.
IUsb derives from IVisaSession.
Methods
| 
                                                     Use of this method is discouraged. All the non-deprecated standard attributes are accessible via properties on the appropriate COM interfaces.  | 
                                            |
| 
                                                     Use of this method is discouraged. All the non-deprecated standard attributes are accessible via properties on the appropriate COM interfaces.  | 
                                            |
| 
                                                     Locks the resource.  | 
                                            |
| 
                                                     Unlocks the resource  | 
                                            |
| 
                                                     Opens the resource. This is the first method on IVisaSession or any of its derived interfaces to be called. In general, you will not call this method because you will use the Resource Manager to create resources.  | 
                                            |
| 
                                                     Closes the resource. Sending the resource's COM object's reference count to zero (and thus destroying the object) also executes a close, but this method may be useful for environments with garbage collection or other facilities that make object lifetimes non-deterministic.  | 
                                            |
| 
                                                    
                                                     Controls the state of the USB REN interface line and, optionally, the remote/local state of the device. This operation asserts or deasserts the USB REN (Remote ENable) interface line according to the specified mode.   | 
                                            |
| 
                                                    
                                                     Sends arbitrary data to a USB device on the default control port. You must be aware of how to use each parameter based on the relevant USB base or class specification, or based on a vendor-specific request definition. Since the USBTMC specification does not currently define any standard control port requests in the direction of host-to-device, this function is intended for use with only vendor-defined requests. However, this function implementation should not check the bmRequestType parameter for this aspect.  | 
                                            |
| 
                                                    
                                                     Used to request arbitrary data from a USB device on the default control port. You must be aware of how to use each parameter based on the relevant USB base or class specification, or based on a vendor-specific request definition.  | 
                                            
Properties
| 
                                                     A numeric version for this component.  | 
                                            |
| 
                                                     The VISA-defined version information for the specification version to which this component complies.  | 
                                            |
| 
                                                     The name of the hardware interface (GPIB, ASRL, etc.).  | 
                                            |
| 
                                                     The board number of the hardware interface.  | 
                                            |
| 
                                                     The type number of the hardware interface.  | 
                                            |
| 
                                                     The current locking state of the interface.  | 
                                            |
| 
                                                     The option string corresponding to the current state of the resource.  | 
                                            |
| 
                                                     The programmatic ID that can be used by COM to create this object.  | 
                                            |
| 
                                                     The VISA resource name of the currently open resource. This name is the canonical version of the resource name and therefore may vary from the resource string used to open/init the resource.  | 
                                            |
| 
                                                     The session type string, such as "INSTR" or "INTFC".  | 
                                            |
| 
                                                     The ID number of the vendor of this software component.  | 
                                            |
| 
                                                     The name of the vendor of this software component.  | 
                                            |
| 
                                                     The I/O timeout in milliseconds for I/O communication on this resource session.  | 
                                            |
| 
                                                     The return value from the last method call on this interface. This property may be useful in Visual Basic, where positive return values, such as warnings and other non-error return values, cannot be retrieved. See the Return Values page for a list of positive return values.  | 
                                            |
| 
                                                     Manufacturer identification number of the USB device.  | 
                                            |
| 
                                                     The manufacturer's name. The value of this attribute should be used for display purposes only and not for programmatic decisions, as the value can be different between VISA implementations and/or revisions.  | 
                                            |
| 
                                                     Model code for the device.  | 
                                            |
| 
                                                     Model name of the device, as a string. The value of this property should be used for display purposes only and not for programmatic decisions, as the value can be different between VISA implementations and/or revisions.  | 
                                            |
| 
                                                     Specifies whether the device is IEEE 488.2 compliant.  | 
                                            |
| 
                                                     The serial number of the USB instrument. The value of this attribute should be used for display purposes only and not for programmatic decisions.  | 
                                            |
| 
                                                     Specifies the USB interface number of this device to which this session is connected.  | 
                                            |
| 
                                                     Specifies the USB protocol number.  | 
                                            |
| 
                                                     Specifies the maximum number of bytes that this USB device will send on the interrupt IN pipe. The default value is the same as the maximum packet size of the interrupt IN pipe.  |