Interface IVisaSession
Description
The base interface for VISA COM I/O resources. This interface has the properties and methods available on all resource types, specifically the lifetime management, locking, identification, and other facilities.
Methods
|
Use of this method is discouraged. All the non-deprecated standard attributes are accessible via properties on the appropriate COM interfaces. |
|
|
Use of this method is discouraged. All the non-deprecated standard attributes are accessible via properties on the appropriate COM interfaces. |
|
|
Locks the resource. |
|
|
Unlocks the resource |
|
|
Opens the resource. This is the first method on IVisaSession or any of its derived interfaces to be called. In general, you will not call this method because you will use the Resource Manager to create resources. |
|
|
Closes the resource. Sending the resource's COM object's reference count to zero (and thus destroying the object) also executes a close, but this method may be useful for environments with garbage collection or other facilities that make object lifetimes non-deterministic. |
Properties
|
A numeric version for this component. |
|
|
The VISA-defined version information for the specification version to which this component complies. |
|
|
The name of the hardware interface (GPIB, ASRL, etc.). |
|
|
The board number of the hardware interface. |
|
|
The type number of the hardware interface. |
|
|
The current locking state of the interface. |
|
|
The option string corresponding to the current state of the resource. |
|
|
The programmatic ID that can be used by COM to create this object. |
|
|
The VISA resource name of the currently open resource. This name is the canonical version of the resource name and therefore may vary from the resource string used to open/init the resource. |
|
|
The session type string, such as "INSTR" or "INTFC". |
|
|
The ID number of the vendor of this software component. |
|
|
The name of the vendor of this software component. |
|
|
The I/O timeout in milliseconds for I/O communication on this resource session. |
|
|
The return value from the last method call on this interface. This property may be useful in Visual Basic, where positive return values, such as warnings and other non-error return values, cannot be retrieved. See the Return Values page for a list of positive return values. |