IVisaSession::HardwareInterfaceName
Description
The name of the hardware interface (GPIB, ASRL, etc.).
VB Prototype
Dim value As String
value = object.HardwareInterfaceName
C++ Prototype
HRESULT get_HardwareInterfaceName(
BSTR* HardwareInterfaceName
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, IVisaSession Overview