| Ivi.Visa Namespace : AddressSpace Enumeration |
'DeclarationPublic Enum AddressSpace Inherits System.Enum
'UsageDim instance As AddressSpace
public enum AddressSpace : System.Enum
public enum class AddressSpace : public System.Enum
| Member | Description |
|---|---|
| PxiAllocation | Physical locally allocated address space. |
| PxiBar0 | PCI memory or I/O address space 0. |
| PxiBar1 | PCI memory or I/O address space 1. |
| PxiBar2 | PCI memory or I/O address space 2. |
| PxiBar3 | PCI memory or I/O address space 3. |
| PxiBar4 | PCI memory or I/O address space 4. |
| PxiBar5 | PCI memory or I/O address space 5. |
| PxiConfiguration | The PCI configuration address space. |
| VxiA16 | The A16 address space of the VXI/MXI bus. |
| VxiA24 | The A24 address space of the VXI/MXI bus. |
| VxiA32 | The A32 address space of the VXI/MXI bus. |
| VxiA64 | The A64 address space of the VXI/MXI bus. |
System.Object
System.ValueType
System.Enum
Ivi.Visa.AddressSpace
Current with Keysight IO Libraries Suite 18