Keysight VISA.NET Help
ReadStatusByte Method (IMessageBasedSession)



Reads the status from the device. For 488.2 instruments, this is the 488.2 status byte.
Syntax
'Declaration
 
Function ReadStatusByte() As StatusByteFlags
'Usage
 
Dim instance As IMessageBasedSession
Dim value As StatusByteFlags
 
value = instance.ReadStatusByte()
StatusByteFlags ReadStatusByte()
StatusByteFlags ReadStatusByte(); 

Return Value

A value that indicates which status byte bits are set.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025