| Ivi.Visa Namespace : IOBuffers Enumeration |
'Declaration<FlagsAttribute()> Public Enum IOBuffers Inherits System.Enum
'UsageDim instance As IOBuffers
[Flags()] public enum IOBuffers : System.Enum
[Flags()] public enum class IOBuffers : public System.Enum
| Member | Description |
|---|---|
| Read | The read (input) buffer. |
| ReadWrite | Both the read (input) and the write (output) buffers. |
| Write | The write (output) buffer. |
System.Object
System.ValueType
System.Enum
Ivi.Visa.IOBuffers
Current with Keysight IO Libraries Suite 18