| Ivi.Visa Namespace : LineState Enumeration |
'DeclarationPublic Enum LineState Inherits System.Enum
'UsageDim instance As LineState
public enum LineState : System.Enum
public enum class LineState : public System.Enum
| Member | Description |
|---|---|
| Asserted | The line is asserted. |
| Unasserted | The line is not asserted. |
| Unknown | It can't be determined if the line is asserted or not. |
System.Object
System.ValueType
System.Enum
Ivi.Visa.LineState
Current with Keysight IO Libraries Suite 18