Keysight VISA.NET Help
NativeErrorCode Class
Members 



The NativeErrorCode class defines constants for each of the standard VISA error status codes that may be returned by an underlying VISA C implementation.
Syntax
'Declaration
 
Public Class NativeErrorCode 
'Usage
 
Dim instance As NativeErrorCode
public class NativeErrorCode 
public ref class NativeErrorCode 
Inheritance Hierarchy

System.Object
   Ivi.Visa.NativeErrorCode

Requirements

Current with Keysight IO Libraries Suite 18

See Also

Reference

NativeErrorCode Members
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025