Keysight VISA.NET Help
ResourceOpenStatus Enumeration



Indicates the success status of an open operation.
Syntax
'Declaration
 
Public Enum ResourceOpenStatus 
   Inherits System.Enum
'Usage
 
Dim instance As ResourceOpenStatus
public enum ResourceOpenStatus : System.Enum 
public enum class ResourceOpenStatus : public System.Enum 
Members
MemberDescription
ConfigurationNotLoaded The session opened successfully, but the specified configuration either does not exist or could not be loaded. The session will use VISA-specified defaults.
DeviceNotResponding The session opened successfully, but the device at the specified address did not respond.
Success The session opened successfully.
Unknown This value is used for an initial state, but will never be returned for a successful open operation.
Inheritance Hierarchy

System.Object
   System.ValueType
      System.Enum
         Ivi.Visa.ResourceOpenStatus

Requirements

Current with Keysight IO Libraries Suite 18

See Also

Reference

Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025