Keysight VISA.NET Help
KeysightVisaEventArgs Class Methods


For a list of all members of this type, see KeysightVisaEventArgs members.

Public Methods
 NameDescription
Public MethodDisposeOverloaded.  Performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this event arguments object, but only if another thread has not already started to dispose of the object.  
Public MethodGetAttributeBooleanOverloaded.  Retrieves the value of the specified attribute from the native C implementation.  
Public MethodGetAttributeByteOverloaded.  Retrieves the value of the specified attribute from the native C implementation.  
Public MethodGetAttributeInt16Overloaded.  Retrieves the value of the specified attribute from the native C implementation.  
Public MethodGetAttributeInt32Overloaded.  Retrieves the value of the specified attribute from the native C implementation.  
Public MethodGetAttributeInt64Overloaded.  Retrieves the value of the specified attribute from the native C implementation.  
Public MethodGetAttributeStringOverloaded.  Retrieves the value of the specified attribute from the native C implementation.  
Top
See Also

Reference

KeysightVisaEventArgs Class
Keysight.Visa Namespace

 

 


© Keysight Technologies 2015-2025