Keysight VISA.NET Help
GetAttributeBoolean(NativeVisaAttribute) Method



A constant that identifies a VISA standard attribute. The type of the attribute must be Boolean.
Retrieves the value of the specified attribute from the native C implementation.
Syntax
'Declaration
 
Public Overloads Function GetAttributeBoolean( _
   ByVal attribute As NativeVisaAttribute _
) As Boolean
'Usage
 
Dim instance As KeysightVisaEventArgs
Dim attribute As NativeVisaAttribute
Dim value As Boolean
 
value = instance.GetAttributeBoolean(attribute)
public bool GetAttributeBoolean( 
   NativeVisaAttribute attribute
)
public:
bool GetAttributeBoolean( 
   NativeVisaAttribute attribute
) 

Parameters

attribute
A constant that identifies a VISA standard attribute. The type of the attribute must be Boolean.

Return Value

The value of the attribute.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025