| Keysight.Visa Namespace : RemoteProtocol Enumeration |
'DeclarationPublic Enum RemoteProtocol Inherits System.Enum
'UsageDim instance As RemoteProtocol
public enum RemoteProtocol : System.Enum
public enum class RemoteProtocol : public System.Enum
| Member | Description |
|---|---|
| HiSlip | The session is connected to a resource on a remote PC using a HiSLIP protocol. |
| NotRemoting | The session is connected to a resource on the local PC. |
| SiclLan | The session is connected to a resource on a remote PC using a SICL-LAN protocol. |
| Vxi11 | The session is connected to a resource on a remote PC using a VXI-11 protocol. |
System.Object
System.ValueType
System.Enum
Keysight.Visa.RemoteProtocol
Current with Keysight IO Libraries Suite 18