Keysight VISA.NET Help
ResourceManager Class Members
Properties  Methods 


The following tables list the members exposed by ResourceManager.

Public Constructors
 NameDescription
Public ConstructorResourceManager ConstructorOverloaded.   
Top
Public Properties
 NameDescription
Public PropertyFindExportedResourcesOnlyDetermines whether only those sessions with property VisaSession.ExportEnabled = true will be returned from the Find and Parse methods. (Keysight Specific)  
Public PropertyImplementationVersion The version of this VISA.NET implementation.  
Public PropertyIOLibrariesPath The full pathname of the Keysight IO Libraries directory used by this implementation of Keysight VISA.NET. The pathname returned varies, depending on whether the process is a 32-bit or 64-bit process. (Keysight Specific)  
Public PropertyIOLibrariesRegistryKey The full pathname of the Keysight IO Libraries registry key used by this implementation of Keysight VISA.NET. The pathname returned varies, depending on whether the process is a 32-bit or 64-bit process. (Keysight Specific)  
Public PropertyManufacturerId The Keysight VISA.NET manufacturer ID - '4095'.  
Public PropertyManufacturerName The VISA.NET vendor name - 'Keysight Technologies, Inc.'.  
Public PropertyReturnAllDetermines whether Find will return all discovered instruments or just those that are in My Instruments list. The default value is false, meaning Find will return only My Instruments. Use Connection Expert to add My Instruments; by default, all locally-connected (non-LAN) instruments and all manually-added instruments are in My Instrument list. (Keysight Specific)  
Public PropertySpecificationVersion The version of the VISA.NET specification with which this VISA.NET implementation complies.  
Public PropertyVisaFrameworkPath The full pathname of the VISA Framework directory used by this implementation of Keysight VISA.NET. The pathname returned varies, depending on whether the process is a 32-bit or 64-bit process. (Keysight Specific)  
Top
Public Methods
 NameDescription
Public MethodDisposeOverloaded.  Performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this implementation of Keysight VISA.NET.  
Public MethodFindFinds all of the VISA.NET resources that match the specified pattern.  
Public MethodOpenOverloaded.  Creates a VISA I/O resource session.  
Public MethodParse Parses a resource string to get extended interface information.  
Top
Protected Methods
 NameDescription
Protected MethodFinalize The default destructor for the ResourceManager class performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this instance of the resource manager.  
Top
See Also

Reference

ResourceManager Class
Keysight.Visa Namespace

 

 


© Keysight Technologies 2015-2025