Keysight VISA.NET Help
IOLibrariesRegistryKey Property



The full pathname of the Keysight IO Libraries registry key used by this implementation of Keysight VISA.NET. The pathname returned varies, depending on whether the process is a 32-bit or 64-bit process. (Keysight Specific)
Syntax
'Declaration
 
Public ReadOnly Property IOLibrariesRegistryKey As String
'Usage
 
Dim instance As ResourceManager
Dim value As String
 
value = instance.IOLibrariesRegistryKey
public string IOLibrariesRegistryKey {get;}
public:
property String^ IOLibrariesRegistryKey {
   String^ get();
}
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025