Keysight VISA.NET Help
StopBits Property (SerialSession)



The number of stop bits used to indicate the end of a frame.
Syntax
'Declaration
 
Public Property StopBits As SerialStopBitsMode
'Usage
 
Dim instance As SerialSession
Dim value As SerialStopBitsMode
 
instance.StopBits = value
 
value = instance.StopBits
public SerialStopBitsMode StopBits {get; set;}
public:
property SerialStopBitsMode StopBits {
   SerialStopBitsMode get();
   void set (    SerialStopBitsMode value);
}
Remarks

The default is Ivi.Visa.SerialStopBitsMode.One.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025