Backplane (BACKPLANE) Resource
This section contains information specific to the Windows product.
This topic describes the PXI/VXI Backplane (BACKPLANE) Resource that encapsulates the operations and properties of the backplane in a PXI or VXIbus system.
BACKPLANE Resource Overview
A VISA BACKPLANE Resource, like any other resource, starts with the basic operations and attributes of the VISA Resource Template. For example, modifying the state of an attribute is done via the operation viSetAttribute, which is defined in the VISA Resource Template.
Although the BACKPLANE resource does not have viSetAttribute listed in its operations, it provides the operation because it is defined in the VISA Resource Template. From this basic set, each resource adds its specific operations and attributes that allow it to perform its dedicated task.
The BACKPLANE Resource lets a controller query and manipulate specific lines on a specific mainframe in a given VXI or PXI system. Services are provided to map, unmap, assert, and receive hardware triggers, and also to assert various utility and interrupt signals. This includes advanced functionality that may not be available in all implementations or all vendors' controllers.
A VXI system with an embedded CPU with one mainframe will always have exactly one BACKPLANE resource. Valid examples of resource strings for this are VXI0::0::BACKPLANE and VXI::BACKPLANE. A multi-chassis VXI system may provide only one BACKPLANE resource total, but the recommended way is to provide one BACKPLANE resource per chassis, with the resource string address corresponding to the attribute VI_ATTR_MAINFRAME_LA. If a multi-chassis VXI system provides only one BACKPLANE resource, it is assumed to control the backplane resources in all chassis.
A PXI system will contain one BACKPLANE resource for each configured chassis, with the resource string address corresponding to the attribute VI_ATTR_PXI_CHASSIS.
|
Some VXI or GPIB-VXI implementations view all mainframes in a VXI system as one entity. In these configurations, separate BACKPLANE resources are not possible. |
BACKPLANE Resource Attributes
|
Attribute Name |
Access Privileges |
Data Type |
Range |
Default |
|
|---|---|---|---|---|---|
Generic BACKPLANE Resource Attributes |
|||||
|
RO |
Global |
ViString |
N/A |
N/A |
|
|
RO |
Global |
ViUInt16 |
0 to FFFFh |
0 |
|
|
RO |
Global |
ViUInt16 |
VI_INTF_VXI |
N/A |
|
|
RW |
Local |
ViUInt32 |
VI_TMO_IMMEDIATE |
2000 msec. |
|
|
RW |
Local |
ViInt16 |
VI_TRIG_SW |
N/A |
|
VXI and GPIB-VXI Specific BACKPLANE Resource Attributes |
|||||
|
RO |
Global |
ViInt16 |
0 to 255 |
N/A |
|
|
RO |
Global |
ViUInt32 |
N/A |
N/A |
|
|
RO |
Global |
ViUInt32 |
N/A |
N/A |
|
|
RO |
Global |
ViUInt16 |
N/A |
N/A |
|
|
RO |
Global |
ViInt16 |
VI_STATE_ASSERTED |
N/A |
|
PXI Specific BACKPLANE Resource Attributes |
|||||
|
RO |
Global |
ViString |
N/A |
N/A |
|
|
RO |
Global |
ViString |
N/A |
N/A |
|
|
RO |
Global |
ViInt16 |
1 to 32767 |
N/A |
|
|
RW |
Local |
ViInt16 |
-1, 1 to 3 |
N/A |
|
|
RW |
Local |
ViInt16 |
-1, 1 to 3 |
N/A |
|
|
RW |
Local |
ViInt16 |
-1, 1 to 3 |
N/A |
|
BACKPLANE Resource Attribute Descriptions
|
Attribute Name |
Description |
|---|---|
Generic BACKPLANE Resource Attributes |
|
|
VI_ATTR_INTF_INST_NAME |
Human-readable text describing the given interface. |
|
VI_ATTR_INTF_NUM |
Board number for the given interface. |
|
VI_ATTR_INTF_TYPE |
Interface type of the given session. |
|
VI_ATTR_TMO_VALUE |
Minimum timeout value to use, in milliseconds. A timeout value of VI_TMO_IMMEDIATE means that operations should never wait for the device to respond. A timeout value of VI_TMO_INFINITE disables the timeout mechanism. |
|
VI_ATTR_TRIG_ID |
Identifier for the current triggering mechanism. |
VXI and GPIB-VXI Specific BACKPLANE Resource Attributes |
|
|
VI_ATTR_MAINFRAME_LA |
This is the logical address of a given device in the
mainframe, usually the device with the lowest logical address. Other possible
values include the logical address of the |
|
VI_ATTR_VXI_TRIG_STATUS |
This attribute shows the current state of the VXI trigger lines. This is a bit vector with bits 0-9 corresponding to VI_TRIG_TTL0 through VI_TRIG_ECL1. |
|
VI_ATTR_VXI_TRIG_SUPPORT |
This attribute shows which VXI trigger lines this implementation supports. This is a bit vector with bits 0-9 corresponding to VI_TRIG_TTL0 through VI_TRIG_ECL1. Keysight VISA also returns 12 to indicate VI_TRIG_PANEL_IN for received triggers and VI_TRIG_PANEL_OUT for asserted triggers on Keysight VXI controllers. |
|
VI_ATTR_VXI_VME_INTR_STATUS |
This attribute shows the current state of the VXI/VME interrupt lines. This is a bit vector with bits 0-6 corresponding to interrupt lines 1-7. |
|
VI_ATTR_VXI_VME_SYSFAIL_STATE |
This attribute shows the current state of the VXI/VME SYSFAIL (SYStem FAILure) backplane line. |
PXI Specific BACKPLANE Resource Attributes |
|
|
VI_ATTR_MANF_NAME |
This string attribute is the chassis manufacturer's name. |
|
VI_ATTR_MODEL_NAME |
This string attribute is the model name of the chassis. |
|
VI_ATTR_PXI_CHASSIS |
This attribute specifies the PXI chassis number of this resource. |
|
VI_ATTR_PXI_TRIG_BUS |
This attribute specifies the segment to use in calls to viAssertTrigger. |
|
VI_ATTR_PXI_SRC_TRIG_BUS |
This attribute specifies the segment to use to qualify trigSrc in calls to viMapTrigger. |
|
VI_ATTR_PXI_DEST_TRIG_BUS |
This attribute specifies the segment to use to qualify trigDest in calls to viMapTrigger. |
BACKPLANE Resource Events
This resource defines the following events for communication with applications, where AP = Access Privilege.
|
VI_EVENT_TRIG - Notification that a trigger interrupt was received from the backplane. For VISA, the only triggers that can be sensed are VXI hardware triggers on the assertion edge (SYNC and ON trigger protocols only). |
||||
|
Event Attribute |
Description |
AP |
Data Type |
Range |
|---|---|---|---|---|
|
Unique logical identifier of the event. |
RO |
ViEventType |
VI_EVENT_TRIG |
|
|
The identifier of the triggering mechanism on which the specified trigger event was received. |
RO |
ViInt16 |
VI_TRIG_TTL0 to VI_TRIG_TTL11; |
|
|
|
||||
|
VI_EVENT_VXI_VME_SYSFAIL - Notification that the VXI/VME SYSFAIL* line has been asserted. |
||||
|
Event Attribute |
Description |
AP |
Data Type |
Range |
|
VI_ATTR_EVENT_TYPE |
Unique logical identifier of the event. |
RO |
ViEventType |
VI_EVENT_VXI_VME_SYSFAIL |
|
|
||||
|
VI_EVENT_VXI_VME_SYSRESET - Notification that the VXI/VME SYSRESET* line has been reset. |
||||
|
Event Attribute |
Description |
AP |
Data Type |
Range |
|
VI_ATTR_EVENT_TYPE |
Unique logical identifier of the event. |
RO |
ViEventType |
VI_EVENT_VXI_VME_SYSRESET |
BACKPLANE Resource Operations
viAssertTrigger (vi, protocol)
viAssertIntrSignal(vi, mode, statusID)
viMapTrigger(vi, trigSrc, trigDest, mode)
viUnmapTrigger(vi, trigSrc, trigDest)
viPxiReserveTriggers(vi, cnt, trigBuses, trigLines, failureIndex)