viMove
                                             This section contains information specific to the Windows product.
 This section contains information specific to the Windows product.
Syntax
viMove(ViSession vi, ViUInt16 srcSpace, ViBusAddress srcOffset, viUInt16 srcWidth, ViUInt16 destSpace, ViBusAddress destOffset, ViUInt16 destWidth,ViBusSize length);
Description
This operation moves data from the specified source to the specified destination. The source and the destination can either be local memory or the offset of the interface with which this INSTR or MEMACC resource is associated. This operation uses the specified data width and address space.
If the ViSession parameter (vi) refers to an INSTR session, the offset parameters specify relative offsets from the start of the instrument’s address space. If the ViSession parameter (vi) refers to a MEMACC session, the offset parameters are absolute offsets from the start of memory in the specified VXI address space.
Valid entries for specifying address space:
| Value | Description | 
|---|---|
| VI_A16_SPACE | Address A16 memory address space of the VXI/MXI bus. | 
| VI_A24_SPACE | Address A24 memory address space of the VXI/MXI bus. | 
| VI_A32_SPACE | Address A32 memory address space of the VXI/MXI bus. | 
| VI_A64_SPACE | Address the A64 address space of VXI/MXI bus. | 
| VI_LOCAL_SPACE | Address the process-local memory (using virtual address). | 
| VI_OPAQUE_SPACE | Addresses potentially volatile data (using a virtual address). | 
| VI_PXI_CFG_SPACE | Address the PCI configuration space. | 
| VI_PXI_BAR0_SPACE – VI_PXI_BAR5_SPACE | Address the specified PCI memory or I/O space. | 
| VI_PXI_ALLOC_SPACE | Access physical locally allocated memory. | 
Valid entries for specifying widths:
| Value | Description | 
|---|---|
| VI_WIDTH_8 | Performs an 8-bit (D08) transfer. | 
| VI_WIDTH_16 | Performs a 16-bit (D16) transfer. | 
| VI_WIDTH_32 | Performs a 32-bit (D32) transfer. | 
| VI_WIDTH_64 | Performs a 64-bit (D64) transfer. | 
The high-level operation viMove operates successfully independently from the low-level operations (viMapAddress, viPeek8, viPeek16, viPeek32, viPeek64, viPoke8, viPoke16, viPoke32, and viPoke64). The high-level and low-level operations are independent regardless of the configured state of the hardware that is used to perform memory accesses.
The length specified in the viMove operation is the number of elements (of the size corresponding to the operation) to transfer, beginning at the specified offset. Therefore, offset + length*size cannot exceed the amount of memory exported by the device in the given space.
If srcSpace is not VI_LOCAL_SPACE, srcOffset is a relative address of the device associated with the given INSTR resource. Similarly, if destspace is not VI_LOCAL_SPACE, destOffset is a relative address of the device associated with the given INSTR resource. srcOffset and destOffset specified in the viMove operation for a MEMACC resource are absolute addresses.
Parameters
| Name | Dir | Type | Description | 
|---|---|---|---|
| vi | IN | ViSession | Unique logical identifier to a session. | 
| srcSpace | IN | ViUInt16 | Specifies the address space of the source. | 
| srcOffset | IN | ViBusAddress | Offset of the starting address or register from which to read. | 
| srcWidth | IN | ViUInt16 | Specifies the data width of the source. | 
| destSpace | IN | ViUInt16 | Specifies the address space of the destination. | 
| destOffset | IN | ViBusAddress | Offset of the starting address or register to which to write.. | 
| destWidth | IN | ViUInt16 | Specifies the data width of the destination. | 
| length | IN | ViBusSize | Number of data elements to transfer, where the data width of the elements to transfer is identical to the source data width. | 
Return Values
| Type ViStatus | This is the function return status. It returns either a completion code or an error code as follows. | 
| Completion Code | Description | 
|---|---|
| VI_SUCCESS | Operation completed successfully. | 
| Error Code | Description | 
| VI_ERROR_BERR | Bus Error occurred during transfer. | 
| VI_ERROR_INV_LENGTH | Invalid length specified. | 
| VI_ERROR_INV_OFFSET | Invalid source or destination offset specified. | 
| VI_ERROR_INV_SESSION | The given session or object reference is invalid (both are the same value). | 
| VI_ERROR_INV_SETUP | Unable to start operation because setup is invalid (due to attributes being set to an inconsistent state). | 
| VI_ERROR_INV_SPACE | Invalid source or destination address specified. | 
| VI_ERROR_INV_WIDTH | Invalid source or destination width specified. | 
| VI_ERROR_NSUP_ALIGH_OFFSET | The specified offset is not properly aligned for the access width of the operation. | 
| VI_ERROR_NSUP_OFFSET | Specified source or destination offset is not accessible from this hardware. | 
| VI_ERROR_NSUP_OPER | The given vi does not support this operation. | 
| VI_ERROR_NSUP_VAR_WIDTH | Cannot support source and destination widths that are different. | 
| VI_ERROR_NSUP_WIDTH | Specified width is not supported. | 
| VI_ERROR_RSRC_LOCKED | Specified operation could not be performed because the resource identified by vi has been locked for this kind of access. | 
See Also
viMoveAsync. Also, see the MEMACC Resource description.