GeneralInstrumentsAPI.proto

Provide various functions that allow you to configure the instrument. The functions are:

Be sure to input the Mandatory settings for the parameters. You may skip the Optional settings.

ImplementConfig

Load the instrument state files to the instrument.

RunOrStopApp

Run or stop data logging feature of the AC Source application.

CheckSupportedModel

Check if the specified instrument model number is supported by the AC Source application.

SetupInstrumentOutputMode

Configure the output mode of the connected instrument.

SetupInstrumentOutputCouplingMode

Configure the output coupling mode of the connected instrument.

SetupInstrumentVoltageRange

Configure the voltage range mode of the connected instrument.

SaveConfig

Save the current instrument state of the connected instrument.

See Also

gRPC Service

Using gRPC Service