Avionics View

Display the available Avionics Standard tests (DO-160 and MIL-STD-704) which are supported by the application. Some revisions, categories and output mode phases settings are supported for both standard tests.

From the Avionics view, you can:

  • Customize the test parameters from the Avionics Standard tests;

  • Customize the lists of tests for execution;

  • Log measurements while running the Avionics Standard tests;

  • Perform quick control modifications;

  • Focus monitoring of specific measurements of interest.

 

To run the Avionics Standard tests, you must have the BV0028B (PathWave BenchVue AC Source Avionics Standard Test Software) license, which consists of the following two license keys:
BV0027B – PathWave BenchVue AC Source Avionics Standard Test Software
KS8000B – PathWave Test Automation Deployment System (TAP_Engine, TAP_RestApi)

Without the BV0028B license, you will only be able to try out the Avionics features in Demo mode. For information on purchasing and installing software licenses, see Software Licensing Options.

Select Test

See Also

Export Avionics Test File

Open Avionics Test File

Run Your Test List

Generate Test Report