CD Arb Waveforms
The available CD Arb waveforms and their associated settings are
as follows:
Square
|
Amplitude - the amplitude or peak value
Offset - the offset from zero
Frequency - the frequency of the square wave
Duty - the duty cycle of the square wave
Phase - the start phase angle of the square wave
Repeat Count - the number of times the waveform repeats
|
Ramp
|
Start Amplitude - the amplitude before the ramp
End Amplitude - the amplitude after the ramp
Delay - the delay after the trigger is received but
before the ramp starts
Ramp Time - the time that the output ramps up
End Time - the time the output remains at the end amplitude
Repeat Count - the number of times the waveform repeats
|
Trapezoid
|
Start/End Amplitude - the amplitude before and after the
trapezoid
Peak Amplitude - the peak amplitude
Start Time - the time before the trapezoid ramps up
Rise Time - the time that the trapezoid ramps up
Peak Time - the time at the peak amplitude
Fall Time - the time that the trapezoid ramps down
End Time - the time the output remains at the end amplitude
Repeat Count - the number of times the waveform repeats
|
StairStep
|
Start Amplitude - the amplitude before the staircase
Single Step Amplitude - the amplitude of a single step
Step Time - the time to complete all of the steps
# of Steps - the total number of staircase steps
Repeat Count - the number of times the waveform repeats
|
Pulse
|
Start/End Amplitude - the amplitude before and after the
pulse
Delay - the delay after the trigger is received but
before the pulse starts
Pulse Time - the time (width) of the pulse
End Time - the time the output remains at the end amplitude
Repeat Count - the number of times the waveform repeats
|