|
|
|
This adjustment creates IF frequency response corrections for bands 1 through 7 of the PSA. The YTF bandwidth is approximately 30 MHz and it will limit the wide IF in Bands 1 through 4.
|
|
This adjustment saves an output file which lists the corrections that were stored in the instrument. The output file is saved at this location:
|
|
Test Equipment |
Model Number |
|---|---|
|
Signal Source |
PSG Models |
|
3.5 mm Cable |
8120-4921 |
|
BNC Cable |
8120-2582 |
|
Type-N (m) to 3.5 mm (f) adapter |
1250-1744 |
|
2.4 mm (f) to 3.5 mm (f) adapter |
11901B |
|
2.4 mm Cable |
8120-6164 |
|
2.4 mm (f) to 2.4 mm (f) adapter |
11900B |