This section lists the test equipment needed to run performance tests and adjustments. Models for each test equipment category are given in order of preference. Alternate models are also listed but should be considered a lower priority. Refer to each individual test for specific setup configurations with required cables and adapters.
All equipment is Keysight, Agilent, or Hewlett Packard unless otherwise specified.
|
Instrument |
Recommended Model |
Alternative Model |
Use1 |
|---|---|---|---|
|
Signal Sources |
|||
|
RF Source 1
|
E4433B Option UND |
E4437B Option UND FW datecode: ³ B.02.24 |
P |
|
RF Source 2 |
E8257D2 |
A, P, T |
|
|
RF Source 3 |
E8257D2 |
8665A/B (std) |
P |
|
Microwave Source 1
|
E8257D2 |
83630A/B, 83640A/B, 83650A/B
PSG3 |
A, P, T |
|
Microwave Source 2
|
PSG3 |
83630A/B, 83640A/B, 83650A/B
PSG3 |
P |
|
Microwave Source 3
|
E8257D2 |
83650A/B Option 001, 008
PSG3 |
A, P, T |
|
Ultra Low Noise Reference Frequency Source |
Wenzel 500-13438 Rev D |
Wenzel 500-13438 Rev C |
P |
|
Function Generator 1 |
For performance verification tests: For adjustments: |
For performance verification tests: For adjustments: |
A, P |
|
Audio Source 1
|
U8903B Audio Analyzer |
Stanford
Research |
P |
|
Counters |
|||
|
Universal Counter |
53230A |
53132A |
P, T |
|
Meters and Power Sensors5 |
|||
|
Digital Multimeter |
3458A |
34470A
|
A, T |
|
Power Meter |
N1914B |
N1914A6 |
A, P |
|
RF Power Sensor
|
N8482A |
8482A7 |
A, P |
|
Power Sensor |
N8481A |
8481A |
P |
|
Microwave
|
N8485A |
8485A |
A, P |
|
Millimeter
|
N8487A |
8487A |
A, P |
|
High
Sensitivity
|
8485D |
|
A, P |
|
High
Sensitivity
|
8487D |
|
A, P |
|
Power Sensor Cable
|
11730A |
|
A, P, |
|
Standards |
|||
|
Frequency Standard |
Microsemi 5071A-C002 |
Microsemi 5071A-C001 |
A, P |
|
50
MHz, |
Z5602B
|
Z5602A
|
A |
|
Attenuators |
|||
|
10 dB |
8496G Option 001, H50 |
8496H Option 001, H50 |
P |
|
1 dB |
8494G Option 001, H50 |
8494H Option 001, H50 |
P |
|
Attenuator Interconnect Kit |
11716A9 |
|
P |
|
Attenuator Driver |
11713E |
11713D |
P |
|
3 dB |
8491A Option 003, H3310 |
8491B Option 003, H3310 |
|
|
6 dB |
8491A Option 006, H3310 |
8491B Option 006, H3310 |
P |
|
10 dB |
8491A Option 010, H3310 |
8491B Option 010, H3310 |
P |
|
10 dB |
8493C Option 010 |
|
A, P |
|
20 dB |
8493C Option 020 |
|
A |
|
20 dB |
8491A Option 020 |
8491B Option 020 |
A |
|
30 dB |
11708A |
|
A,P |
|
Terminations |
|||
|
Type-N (m) |
909A Option 012 |
|
P, T |
|
50 W 3.5 mm (f) |
909D Option 011 |
|
P |
|
50 W 2.4 mm (f)
|
85138B |
|
P |
|
50 W BNC (m) |
1250-0207 |
|
P |
|
Miscellaneous Devices |
|||
|
RF Power Splitter |
11667A |
|
P |
|
Microwave
|
11667B |
|
P |
|
Millimeter
|
11667C |
|
P |
|
Directional Bridge |
86205A |
|
P |
|
Directional Coupler |
87300B |
87300C |
P |
|
DC Probe |
11002A |
11003A |
A |
|
High Frequency Probe |
85024A |
|
T |
|
Bias Adjustment Board |
E4440-60041 |
|
A |
|
Cables |
|||
|
3.5 mm (m) to 3.5 mm (m)
|
8120-4921 |
|
A, P |
|
2.4 mm (f) to 2.4 mm (m)
|
8120-6164 |
|
A, P |
|
Type-N
|
11500C |
|
A, P, T |
|
BNC
|
8120-2582 |
10503A |
A, P, T |
|
Filters |
|||
|
50 MHz Low Pass |
0955-0306 |
Telonic
Berkeley |
P, T |
|
300 MHz Low Pass
|
0955-0455 |
Telonic
Berkeley |
P |
|
1.8 GHz Low Pass
|
0955-0491 |
RLC
Electronics |
P |
|
4.4 GHz Low Pass
|
9135-0005 |
K
+ L Microwave |
P |
|
1 GHz Low Pass |
0955-0487 |
RLC
Electronics |
P |
|
1.0001 GHz Notch
|
Trilithic CFN-2-1000.1 |
|
P |
|
Adapters |
|||
|
Type-N (f) to Type-N (f) |
1250-1472 |
|
P |
|
Type-N (m) to Type-N (m) |
1250-1475 |
|
P |
|
Type-N (f) to BNC (m) |
1250-1477 |
|
P, T |
|
Type-N (m) to BNC (m) |
1250-1473 |
|
P, T |
|
Type-N (m) to 3.5 mm (m) |
1250-1743 |
|
P |
|
Type-N (m) to BNC (f) |
1250-1476 |
|
P |
|
3.5 mm (f) to 3.5mm (f)
|
83059B |
1250-1749 |
P |
|
3.5 mm (m) to 3.5 mm (m)
|
1250-1748 |
|
P |
|
3.5 mm (f) to 3.5mm (f) |
1250-1749 |
|
P |
|
2.4 mm (f) to 3.5 mm (m)
|
11901D |
|
A, P |
|
2.4 mm (f) to 2.4 mm (f)
|
11900B |
|
A, P |
|
3.5 mm (f) to Type-N (f) |
1250-1745 |
|
A, P |
|
3.5 mm (f) to 2.4 mm (f)
|
11901B |
|
P |
|
BNC (m) to SMA (f) |
1250-1700 |
|
P |
|
Type-N (m) to 3.5 mm (f)
|
1250-1744 |
|
P |
|
Type-N (f) to 2.4 mm (f) |
11903B |
|
A, P |
|
Type-N (m) to 2.4 mm (f)
|
11903D |
|
P |
|
Type-N (f) to 3.5 mm (m) |
1250-1750 |
|
A, P |
|
BNC Tee (BNC f,m,f) |
1250-0781 |
|
A, P |
|
SMB (f) to BNC (f) |
1250-1236 |
|
A, P |
|
BNC (f) to SMA (m) |
1250-1200 |
|
A, P |
|
BNC (f) to Dual Banana |
1251-2277 |
|
A, P |
|
3.5 mm (f) to Type-N (m) |
08485-60005 |
|
A, P |
|
2.4 mm (f) to Type-N (m) |
08487-60001 |
|
A, P |
|
Optional Equipment |
|||
|
10 MHz Distribution Amplifier
|
Microsemi 5087B |
Microsemi 5087A |
A, P |
|
Aeroflex Weinschel Crown, 2.4 mm (m)
|
7005A-13 |
A, P, T |
|
A = Adjustments, P = Performance Testing, T = Troubleshooting
One PSG with Option 567, 1EA/1EU, 1E1, 007, and UNX or UNR or UNY can be used as the Microwave Source #1, RF Source #2, and RF Source #3. (Option 007 Analog Ramp Sweep is required for Frequency Response Adjustments.)
|
|
|
(One sweeper requires Option 1E1 for PSA Option 110 testing.) |
|
When ordering a new STD or CFT power sensor from Keysight to be used with the N7800A series applications, order with Option 1A7. The 1A7 option provides an ISO17025 calibration and includes calibration data. When re-calibrating your STD or CFT power sensor for use with the N7800A series applications, we recommend the Keysight ISO17025 calibration.
N1914A power meters with serial number prior to MY53040007 require Service Note N1914A-07 which fixes a power supply ground loop. The ground loop injects noise into the measurement circuits which can cause unstable measurements at low (-30 dBm) power levels.
The 8482A power sensor uses cal factors to compensate the power sensor for frequency response errors. Cal factors are stated in percentages. The 8482A factory cal factor uncertainty ranges from 2.2% to 3.1%. The cal factor uncertainty can be reduced to < 2.0% by using metrology grade calibration techniques. The power sensor cal factor uncertainty becomes one component of the Verification Test uncertainty analysis. Lower cal factor uncertainties will translate to wider test margins.
When using the 10 MHz External Reference with performance tests, be sure to update the Additional Properties in TME to the correct Frequency Accuracy in parts per million (ppm). For example, if overall accuracy is 9e-12, the equivalent is 9e-6 ppm. Refer to the Additional Properties section in the N7800A TME Help for instructions. (Does not apply to adjustments.)
The step attenuators should be permanently joined via the 11716A Interconnect Kit as shown in the diagram.
The step attenuator combination should have each attenuator setting characterized by a metrology lab at 50 MHz. This characterization can be ordered through Keysight Technologies as an Option H50 Calibration.
The following tables show which sections of the 10 dB and 1 dB step attenuators are utilized for each attenuator setting. The tables also list the Recommended Uncertainty for each attenuator setting. A larger number will result in larger overall test uncertainties which could affect the test pass/fail rate.
The interconnect cable should NEVER be disconnected once the loss characterization is performed.
|
Nominal Attenuation |
Attenuator Section |
Recommended |
|||
|
#1 |
#2 |
#3 |
#4 |
||
|
0 |
Off |
Off |
Off |
Off |
0 (Reference) |
|
1 |
On |
Off |
Off |
Off |
< 0.005 |
|
2 |
Off |
On |
Off |
Off |
< 0.005 |
|
3 |
On |
On |
Off |
Off |
< 0.005 |
|
4 |
Off |
Off |
Ona |
Off |
< 0.005 |
|
5 |
On |
Off |
On |
Off |
< 0.005 |
|
6 |
Off |
On |
On |
Off |
< 0.005 |
|
7 |
On |
On |
On |
Off |
< 0.005 |
|
8 |
Off |
Off |
On |
On |
< 0.005 |
|
9 |
On |
Off |
On |
On |
< 0.005 |
|
10 |
Off |
On |
On |
On |
< 0.005 |
|
11 |
On |
On |
On |
On |
< 0.005 |
|
Nominal Attenuation |
Attenuator Section |
Recommended |
|||
|
#1 |
#2 |
#3 |
#4 |
||
|
0 |
Off |
Off |
Off |
Off |
0 (Reference) |
|
10 |
On |
Off |
Off |
Off |
< 0.010 |
|
20 |
Off |
On |
Off |
Off |
< 0.015 |
|
30 |
On |
On |
Off |
Off |
< 0.020 |
|
40 |
Off |
Off |
Ona |
Off |
< 0.025 |
|
50 |
On |
Off |
On |
Off |
< 0.030 |
|
60 |
Off |
On |
On |
Off |
< 0.035 |
|
70 |
On |
On |
On |
Off |
< 0.040 |
|
80 |
Off |
Off |
On |
On |
< 0.046 |
|
90 |
On |
Off |
On |
On |
< 0.055 |
|
100 |
Off |
On |
On |
On |
< 0.065 |
|
110 |
On |
On |
On |
On |
< 0.075 |
|
|
8491A Option H33 is a fixed attenuator which has been characterized to have a VSWR £ 1.05:1 at 50 MHz. A VSWR of 1.05:1 is critical to test Input Attenuator Switching Uncertainty, Display Scale Fidelity, and Absolute Amplitude Accuracy performance tests. Any 8491A/B attenuator can be mapped into this device if the VSWR at 50 MHz has been characterized to be £ 1.05:1. When mapping the attenuator, to indicate that is meets the required specification, the Option H33 checkbox will need to be checked in the configure test station Administration screen.
To ensure data integrity for measurements carried out with TME (Test Management Environment), the following verification checks are carried out at the beginning of each test run. The checks are only performed on devices that require calibration data which directly affect the test results.
The following table lists the standard checks performed by default:
| Device | Parameter Name and Description | Limits | A
Failure Affects: |
|---|---|---|---|
|
Power Sensor |
CalFactor(%)
|
Must be ³
10% and £
150% at all points |
All test runs |
|
Uncertainty(%)
|
Must be > 0 and £ 10% at all points |
Test runs guard banded by measurement uncertainty only |
|
|
ReflectCoeff(Mag)
|
Must be >
0 and < 0.5 |
Test runs guard banded by measurement uncertainty only |
|
|
Power Sensor |
LowBandCalFactor(%)
|
Same tests as for CalFactor(%) on a one-range power sensor |
All test runs |
|
HighBandCalFactor(%)
|
Same tests as for LowBandCalFactor(%) |
All test runs |
|
|
LowBandUncertainty(%)
|
Same tests as for Uncertainty(%) on a one-range power sensor |
Test runs guard banded by measurement uncertainty only |
|
|
HighBandUncertainty(%)
|
Same tests as for LowBandUncertainty(%) |
Test runs guard banded by measurement uncertainty only |
|
|
ReflectCoeff(Mag)
|
Same tests as for ReflectCoeff(Mag) on a one-range power sensor |
Test runs guard banded by measurement uncertainty only |
|
|
Step Attenuator |
Atten(dB)
|
Must be within 1 dB of the nominal attenuation.
|
All test runs |
|
Uncert(dB)
|
See the attenuator tables above for the specification |
Test runs guard banded by measurement uncertainty only |
|
|
ReflSize
|
Must be > 0 and < 0.5 at all points |
Test runs guard banded by measurement uncertainty only |
The 10 MHz connections shown in the test diagrams are displayed as a direct connection between the signal analyzer and the signal source. If the test equipment is used as a dedicated test system with multiple signal sources, it might be more practical to employ a 10 MHz Distribution Amplifier. The 10 MHz Distribution Amplifier (Keysight 5087A for example) allows a single 10 MHz Reference to be connected to multiple 10 MHz inputs. The Distribution Amplifier output power should be adjusted for a nominal +7 dBm with an input power of +3 dBm.
The following diagram shows how the Distribution Amplifier would be connected to the test system.
|
|
Distribution amplifiers tend to add large AC power related spurs onto the 10 MHz reference signal. This can cause false failures in the Noise Sidebands < 50 kHz Offsets test at the 100 Hz offset. If a failure is encountered in the Noise Sidebands < 50 kHz Offsets test, then remove the distribution amplifier from the signal path. |