The overload detector is in the first IF in the A20 Low Band. It is used as a warning when a high input level outside the viewing span is compressing the first mixer. It can also be used as a diagnostic tool.
This adjustment should be performed after replacing the A20 assembly.
|
|
This adjustment saves an output file which lists the corrections that were stored in the instrument. The output file is saved at this location:
|
|
Test Equipment |
Model Number |
|---|---|
|
Synthesized Sweeper |
PSG Models |
|
Type-N Cable |
11500C |
|
Type-N
(f) to 3.5 mm (f) adapter |
1250-1745 |
|
2.4 mm (f) to Type-N (f) adapter |
11903B |