|
|
The measurement will only be made if Option 239 (EMI Measurement Application) is present in the PSA. |
The PSA resolution bandwidths are implemented in DSP.
To measure the Shape factor a signal is input into the PSA. The filter shape will be drawn on the PSA display. The test will then read the 101 trace points and overlay the points on the CISPR mask.
Click here for troubleshooting.
|
Test Equipment |
Model Number |
|---|---|
|
Signal Source |
PSG Models |
|
BNC Cable |
8120-2582 |
|
3.5 mm (f) to 3.5 mm (f) Cable |
11500E |
|
3.5 mm (f) to 3.5 mm (f) adapter |
83059B |
|
3.5 mm (f) to Type-N (m) adapter |
1250-1744 |