This test measures the Third-Order Intermodulation distortion produced by two input signals, and computes the Third Order Intercept (TOI) point.
Two signals separated by 100 kHz are combined in a directional bridge, or directional coupler, and are input to the PSA. Mixing products will appear on the PSA above and below the two fundamental frequencies. These mixing products are Third Order products which are located at 2*F1-F2, and 2*F2-F1, where F1 < F2 . The PSA measures the amplitude of the lower and upper distortion products relative to the fundamental frequency. TOI is computed using the higher amplitude mixing product.
Testing begins by turning on one signal source and measuring the signal level at the splitter output with a power meter. The other splitter output is connected to the PSA input. The signal amplitude is measured on the PSA. The second signal source is turned on and its amplitude is adjusted to match that of the first signal. The distortion products are then measured relative to the fundamental amplitude. The Intercept point is calculated as: TOI = Mixer Level + Distortion (dBc)/2.
In the 3 Hz to 3 GHz band, a filter is used to attenuate signal generator second harmonic product (2*F1). If a low pass filter was not used, the source second harmonic would artificially increase the distortion product. Above 3 GHz, the analyzer provides internal preselection so the source does not require an external filter.
Click here for troubleshooting.
|
Test Equipment |
Model Number |
|---|---|
|
Synthesized Sweeper |
PSG Models |
|
Power Meter |
N1914B |
|
Power Sensor |
N8485A |
|
Power Splitter |
11667B |
|
Directional Bridge |
86205A |
|
Directional Coupler |
87300B |
|
10 dB Attenuator |
8493C (Option 010) |
|
BNC Cable (2 required) |
8120-2582 |
|
3.5 mm Cable (2 required) |
8120-4921 |
|
50 MHz Low Pass Filter |
0955-0306 |
|
1.8 GHz Low Pass Filter |
0955-0491 |
|
3.5 mm (f) to 3.5 mm (f) adapter |
83059B |
|
BNC (m) to SMA (f) adapter |
1250-1700 |
|
Type-N (m) to Type-N (m) adapter |
1250-1475 |
|
Type-N (m) to BNC (f) adapter |
1250-1476 |
|
Type-N (m) to 3.5 mm (m) adapter |
1250-1743 |
|
Type-N (m) to 3.5 mm (f) adapter |
1250-1744 |
|
3.5 mm (m) to 3.5 mm (m) adapter |
1250-1748 |
|
2.4 mm (f) to 3.5 mm (f) adapter |
11901B |
|
2.4 mm (f) to 3.5 mm (m) adapter |
11901D |
|
3.5 mm (f) to Type-N (m) |
08485-60005 |