IF Input Accuracy Troubleshooting

Related Adjustments:

This test inputs a 321.4 MHz, -10 dBm signal into the PSA IF Input port. The PSA marker should read -10 dBm when the PSA is placed in External Mixing mode. If the IF input accuracy test fails, it could mean the A10 Third Converter is defective.