Residual Responses Troubleshooting

Related Adjustments:

If the residuals test fails, check the results of the DANL Performance Test. If DANL is out of spec, there is a good possibility that the high average noise level is causing the residuals test to indicate a false failure.

Also make sure that the 50 ohm load is attached to the analyzer RF Input connector. Failures are usually caused by loose or defective cables or loose shielding on an assembly.

See the PSA Service Guide for troubleshooting information.