The performance verification tests are designed to provide the highest level of confidence that the instrument being tested conforms to published, factory-set specifications. The tests are designed to test an instrument operating within the temperature range defined by the instrument specifications. Some repairs require a performance test to be run after the repair. If the instrument is unable to pass any of the performance tests, adjustments or further repairs are needed.
Gain Compression (see Note below)
IF Phase Ripple (Option B7J) (see Note below)
Noise Sidebands < 50 kHz Offsets (see Note below)
Noise Sidebands > 50 kHz Offsets (see Note below)
|
|
This test is run from the Normal Variant in TME. For more information on variants, click here. |