The Residual FM test verifies that the instrument meets the published specifications for residual FM. The signal source is provided by a synthesized signal generator producing a CW signal. The source amplitude is set to a constant value throughout the test. The FM modulation on the input signal is measured. Then the residual FM is calculated.
See Application Note 150-1 (5954-9130) for more information on this FM modulation model.
Click here for troubleshooting.
Related adjustments: None
|
Test Equipment |
Recommended Model Number |
|---|---|
|
RF Source 2 |
E8257D |
|
Cable, Type-N |
11500C |
|
Cable, BNC |
8120-2582 |