N7812A Test Equipment

The Agilent Recommended Test Plan has become the Factory Recommended Test Plan. Refer to the Test System Variants section of Getting Started for more information.

This topic shows the equipment required to run the performance verification and adjustment tests. Some tests (for example Flatness) can use various model numbers of a particular equipment type. The Recommended Model will provide the best results. However, the Alternative Model is an acceptable substitute.

Not all of the listed test equipment needs to be connected to perform an individual test. To run a test, only the equipment specified for that test needs to be connected.

The validity of performance verification and adjustment measurements depend in part on the accuracy of the required test equipment. Verify proper calibration of test equipment before running tests with this software.

The following sections are included in this topic:

Required Test Equipment

Test Equipment

Recommended Model

Alternative Model

Sources

RF Source 1

E8257D1

E8257C
E8267C/D
83620B
83623B
83630A/B/L
83640A/B/L
83650A/B/L
E8663B Option 509

RF Source 2

E8257D1

E8257C
E8267C/D
8663A
E8663B

RF Source 3

  • Normal Variant only

E4433B Option UND

E4430B Option UND
E4431B Option UND
E4432B Option UND
E4434B Option UND
E4435B Option UND
E4436B Option UND
E4437B Option UND

RF Source 4

  • Normal Variant only

8665B

8665A

RF Source 5

  • Factory Recommended Variant only

E8257D1

E8257C
E8267C/D
E8663B
8665A/B

Secondary Source

33250A function generator

E8257C/D
E8267C/D
8663A
E8663B

Analyzers

Network analyzer

N5245B PNA-X

N5241A/B
N5242A/B
N5244A/B
N5245A
N5247A/B

N5232A/B
N5234A/B
N5235A/B

N5222A/B
N5224A/B
N5225A/B
N5227A/B

N5230A/C
E5071C
E8364B/C
E8363B/C
E8361A/C
8753D/E
8753ES/ET

Counters

Frequency counter

53230A

53220A
53132A
53131A

Meters and Power Sensors (See below for calibration service ordering guidelines.)

Digital multimeter

  • Required for adjustments only

3458A

 

Power meter

N1914A2

N1912A
E4419A/B
EPM-442A

Power sensor

  • 2 required

N8482A

N8482A Option CFT
8482A
8482A Option H84

Power sensor, low power

  • Required for adjustments only

8481D


Standards

Frequency standard

Microsemi 5071A

5061B

Attenuators

10 dB
Step Attenuator3

 8496G Option 001, H50

 8496H Option 001, H50

1 dB
Step Attenuator3

 8494G Option 001, H50

 8494H Option 001, H50

Attenuator Interconnect Kit3

 11716A

 

Attenuator Driver

 11713B

 11713A

6 dB
Fixed Attenuator

  • 2 required

 8491A Option 006

8491B Option 006
8491C Option 006

20 dB
Fixed Attenuator

8491A Option 020

 

30 dB
Fixed Attenuator

  • Used with the 8481D power sensor

11708A

 

Filters

50 MHz Low Pass

0955-0306

 

1.0001 GHz Notch

Trilithic CFN-2-1000.1

 

Miscellaneous Devices

50 Ω termination

909A Option 012

 

Power splitter

11667A

 

Directional bridge

86205A

8721A

Calibration kit, Type-N

85054B

85032A/B/C/D/E/F

Cables

Type-N

  • 2 required

11500C

 

BNC

  • 3 required

 8120-2582

10503A

Adapters

Type-N (f) to Type-N (f)

1250-1472

 

Type-N (m) to Type-N (m)

1250-1475

 

Type-N (f) to BNC (m)

1250-1477

 

Type-N (m) to BNC (f)

1250-1476

 

Type-N (m) to BNC (m)

1250-1473

 

3.5 mm (f) to Type-N (f)

  • For 3.5 mm source

1250-1745

 

Type-N (f) to 2.4 mm (f)

  • For 2.4 mm source

11903B

 

7 mm to Type-N (f)

Included in cal kit

 

Table Footnotes

  1. E8257D with Options 1EA/1EU, 1E1, 007, and UNX or UNR or UNY can be used as RF Source #1, RF Source #2, and RF Source #5.

  2. N1914A power meters with serial number prefix prior to MY53040007 require Service Note N1914A-07 which fixes a power supply ground loop. The ground loop injects noise into the measurement circuits which can cause unstable measurements at low (–30 dBm) power levels

  3. The step attenuators should be permanently joined via the 11716A Interconnect Kit as shown in the diagram.

    Step Attenuator Loss Characterization

    The step attenuator combination should have each attenuator setting characterized by a metrology lab at 50 MHz. The following tables show which sections of the 10 dB and 1 dB step attenuators are utilized for each attenuator setting. The tables also list the Allowable Uncertainty for each attenuator setting.

    The interconnect cable should NEVER be disconnected once the loss characterization is performed.

    1 dB Step Attenuator

    Nominal Attenuation
    (dB)

    Attenuator Section

    Recommended
    Uncertainty
    (dB)

    #1
    (1 dB)

    #2
    (2 dB)

    #3
    (4 dB)

    #4
    (4 dB)

    0

    Off

    Off

    Off

    Off

    0 (Reference)

    1

    On

    Off

    Off

    Off

    < 0.005

    2

    Off

    On

    Off

    Off

    < 0.005

    3

    On

    On

    Off

    Off

    < 0.005

    4

    Off

    Off

    Ona

    Off

    < 0.005

    5

    On

    Off

    On

    Off

    < 0.005

    6

    Off

    On

    On

    Off

    < 0.005

    7

    On

    On

    On

    Off

    < 0.005

    8

    Off

    Off

    On

    On

    < 0.005

    9

    On

    Off

    On

    On

    < 0.005

    10

    Off

    On

    On

    On

    < 0.010

    11

    On

    On

    On

    On

    < 0.010

    1. TME requires that Section 3 be characterized.

     

    10 dB Step Attenuator

    Nominal Attenuation
    (dB)

    Attenuator Section

    Recommended
    Uncertainty
    (dB)

    #1
    (10 dB)

    #2
    (20 dB)

    #3
    (40 dB)

    #4
    (40 dB)

    0

    Off

    Off

    Off

    Off

    0 (Reference)

    10

    On

    Off

    Off

    Off

    < 0.010

    20

    Off

    On

    Off

    Off

    < 0.015

    30

    On

    On

    Off

    Off

    < 0.020

    40

    Off

    Off

    Ona

    Off

    < 0.025

    50

    On

    Off

    On

    Off

    < 0.030

    60

    Off

    On

    On

    Off

    < 0.035

    70

    On

    On

    On

    Off

    < 0.040

    80

    Off

    Off

    On

    On

    < 0.046

    90

    On

    Off

    On

    On

    < 0.055

    100

    Off

    On

    On

    On

    < 0.058

    110

    On

    On

    On

    On

    < 0.064

    1. TME requires that Section 3 be characterized.

Guidelines for Ordering Power-Sensor Calibration Service

Use the following guidelines to ensure power sensors used by the N7800A application receive the correct calibration service:

  1. Order Option 1A7 when ordering new power sensors that will be used as working standards in N7800A TME calibrations.

  2. In the Americas region, order the Keysight Cal + Measurement Uncertainty for power sensor recalibration.

  3. Outside the Americas region, order ISO 17025/ILAC-G8 calibration service for power sensor recalibration.

  4. When ordering periodic calibration for instruments used as lab standards in the N7800A software, we recommend using “Keysight calibration + uncertainties” for power sensors, and “Keysight calibration + uncertainties + guardbanding” for all other items (please visit Selecting the Right Calibration Services). The N7800A software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options in this table provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). Please order Option H99 to get data on a CD for easy import into the N7800A (avoids manual entry). The overall resulting N7800A measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N7800A calibration application are summarized in the specials calibration matrix which can be found at the Recommended Lab Standards and Special Cal Options website.

  5. The Keysight Option H99 is a special option for the Roseville Service Center [only] which provides a CD with calibration data included as a .csv file in TME N7800A format for all power sensors used with the N7800A TME application. N7800A TME is SSU calibration software used across Keysight SSU and by many self-maintainers. H99 must be requested from the Roseville SSU upon re-calibration only of any previously purchased power sensor and not for new purchases of BID Power Sensors. This option provides for adding the calibration data to a CD and may be ordered in addition to any other required or requested Std Lab Calibration option (must also be ordered in addition to H99). Option H99 is recommended but not required.

    The following models are not supported by Option H99 (calibration data on a CD in .csv format):

    • E9304A-H18
    • E9304A-H19
    • E9304A-H84
    • E9400A-H25
    • N8486AQ
    • N8486A

Power Sensor & Power Meter Calibration & Zeroing Operation

The calibration and zeroing operation of a power sensor and power meter are done automatically by the software. Each operation is valid for 2 hours.

When a power sensor is needed for a given test, you will be asked to connect it to the appropriate power meter channel and POWER REF input in order to do the calibration and zeroing operation. The time stamp of the operation is then logged based on the serial numbers. The next time that a test requires the use of these two pieces of equipment, the last operation time stamp (if one exists) is checked to determine if a new calibration and zeroing operation is needed.

Disconnecting the power sensor from the channel port or powering down the power meter will invalidate a calibration and zeroing operation; closing the application will not.

An existing logged time stamp will not be affected by these actions.

Self Alignment

A self -alignment procedure is automatically run when the E4406A VSA is turned on. The instrument will automatically run a new self-alignment procedure when 24 hours have elapsed.

When a test requires a self alignment, it will run it. The time stamp of the procedure is then logged based on the instrument serial number. When another test requires a self alignment, it first checks the last self-alignment time stamp to determine if a new procedure is needed.

Closing the application does not cause the deletion of the time stamp which is logged against the self alignment procedure.

Warmup Times

Please allow sufficient warmup time for the test equipment. Refer to the specified operating temperature range.

Calibration Data Validation

Standard Checks

To ensure data integrity for measurements carried out with TME (Test Management Environment), the following verification checks are carried out at the beginning of each test run. The checks are only performed on devices that require calibration data which directly affect the test results.

The following table lists the standard checks performed by default:

Device Parameter Name and Description Limits A Failure Affects:

Noise Source

NoiseRatio(dB)
The extended noise ratio, in dB

Must be > and ≤ 30 at all points

All tests runs

Power Sensor

CalFactor(%)
The calibration factor, as a percentage

Must be ≥ 10% and ≤ 150% at all points.
Must not be 100% (the default) at all points.

All test runs

Uncertainty(%)
The uncertainty of the calibration factor, as a percentage

Must be > 0 and ≤ 3% at all points

Test runs guard banded by measurement uncertainty only

ReflectCoeff(Mag)
The magnitude of the reflection coefficient

Must be > 0 and < 0.5 at all points

Test runs guard banded by measurement uncertainty only

Power Sensor
(Wide Band)

LowBandCalFactor(%)
The calibration factor, as a percentage, for the low band

Same tests as for CalFactor(%) on a one-range power sensor

All test runs

HighBandCalFactor(%)
The calibration factor, as a percentage, for the high band

Same tests as for LowBandCalFactor(%)

All test runs

LowBandUncertainty(%)
The uncertainty of the calibration factor, as a percentage, for the low band

Same tests as for Uncertainty(%) on a one-range power sensor

Test runs guard banded by measurement uncertainty only

HighBandUncertainty(%)
The uncertainty of the calibration factor, as a percentage, for the high band

Same tests as for LowBandUncertainty(%)

Test runs guard banded by measurement uncertainty only

ReflectCoeff(Mag)
The magnitude of the reflection coefficient

Same tests as for ReflectCoeff(Mag) on a one-range power sensor

Test runs guard banded by measurement uncertainty only

Step Attenuator

Atten(dB)
The attenuation, in dB

Must be within 1 dB of the nominal attenuation. Must not all be exactly equal to the nominal attenuation (the default) at all points except zero. Zero step is the reference and must be zero.

All test runs

Uncert(dB)
The uncertainty of the attenuation, in dB

Must be > 0 and ≤ 0.1 dB at all points except zero. Zero step is the reference and must be zero.

Test runs guard banded by measurement uncertainty only

ReflSize
The reflection coefficient magnitude

Must be > 0 and < 0.5 at all points

Test runs guard banded by measurement uncertainty only

Test Plan Specific Checks

In addition to the standard checks carried out, the following additional limits affecting measurement uncertainty are verified for the E4406A VSA performance verification test plan.

Failure to comply with either set of limits will result in test data being labeled Invalid in both the TME interface and in any report produced from the data.

Power Sensors

Device

Models

Parameter
Name

Frequency
Range

Limits

A Failure
Affects:

PowerSensor1

8482A

Uncertainty(%)

1 MHz – 4 GHz

≤ 1.2

Test runs guard banded by measurement uncertainty only

ReflectCoeff(Mag)

7 MHz – 4 GHz

 ≤ 0.130435

Step Attenuators

Device

Models

Parameter Name

Attenuator Step

Limits

A Failure
Affects:

StepAttenuator10-1

8496G

Uncert(dB)

0

= 0

Test runs guard banded by measurement uncertainty only

10

≤ 0.0102

20

≤ 0.0154

30

≤ 0.0206

40

≤ 0.0258

50

≤ 0.031

60

≤ 0.0362

70

≤ 0.0414

80

≤ 0.0466

90

≤ 0.0518

100

≤ 0.057

110

≤ 0.0622

ReflSize

All

≤ 0.0909091

StepAttenuator1-1

8494G

Uncert(dB)

All except zero. Zero step is the reference and must be zero.

≤ 0.01

ReflSize

All

≤ 0.0909091