IF Frequency Response UWBIF Full Bypass Path Adjustment

This adjustment applies to the following models:

The goal of this adjustment is to generate corrections for the IF band shape in Full Bypass Path (Option FBP). Option FBP allows both LNP and MPB to be enabled. A separate set of IF corrections are necessary for this RF Path. Since Full Bypass Path only affects frequencies above 3.6 GHz, only Bands 1, 2, 3, 4, 5, 6 are adjusted. This adjustment takes several hours, so it was separated from the same adjustment for Preselector Bypass Path (Option MPB).

In this adjustment, a –10.00 dBm signal is applied to the DUT. A reference amplitude is taken at the IF center frequency. The source frequency is then changed to a series of offset frequencies within the span of the IF. At each offset frequency, the input amplitude is maintained at –10.00 dBm, and the signal amplitude is measured by the DUT. The offset amplitude is subtracted from the reference amplitude. The resulting envelope created by all the offset amplitudes is the uncorrected IF Frequency Response.

Click here for troubleshooting.

Required Test Equipment

Test Equipment

Recommended Model Number

Microwave Signal Generator #1

PSG Models
(see equipment list)

Power Meter

N1914B

Microwave Power Sensor

N8485A 

Microwave Power Splitter

11667B

Coaxial Cable, 3.5 mm (m) to 3.5 mm (m)

11500F

BNC Cable

8120-1840 

Type-N (m) to 3.5 mm (m) adapter

1250-1743

3.5 mm (f) to 3.5 mm (f) adapter
(for 3.5 mm source)

83059B

3.5 mm (f) to 2.4 mm (f) adapter
(for 2.4 mm source)

11901B

3.5 mm (f) to Type-N (m)
(8485A adapter)

08485-60005

 

Connection Setups

In the following setups, cables are designated as solid lines and direct connections are designated as dashed lines.

 

Power Meter Calibration

 

IF Frequency Response UWBIF Full Bypass Path Adjustment Setup