N7814A Test Equipment

This section lists the test equipment needed to run performance tests and adjustments. Models for each test equipment category are given in order of preference. Alternate models are also listed but should be considered a lower priority. Refer to each individual test for specific setup configurations with required cables and adapters.

Required Test Equipment

Instrument

Recommended Model1

Alternative Model1

Use2

Sources

Microwave
Signal Generator #1

E8257D Options 567, 1EA/1EU, 1E1

  • Option 007 (Analog Ramp Sweep) required for Frequency Response Adjustments.

PSG3

For Adjustments only:4
83630A/B/L Opt 001, 008
83640A/B/L Opt 001, 008
83650A/B/L Opt 001, 008

A, P, T

Microwave
Signal Generator #2

  • Only required for Third Order Intermodulation and Gain Compression.

E8257D Opt 1EA/1EU

PSG3

83630A/B/L4 Opt 001, 008
83640A/B/L4 Opt 001, 008
83650A/B/L4 Opt 001, 008

P

Low Noise
Signal Generator

  • One PSG may be used for
    multiple sources. See footnote below.

E8257D Options UNR, UNX, or UNY

PSG3 Options UNR, UNX, or UNY

A, P, T

RF Signal Generator

  • One PSG may be used for
    multiple sources. See footnote below.

E8257D Options UNR, UNX, or UNY

  • Option 1E1 required for CXA Option C75 Frequency Response test and adjustment.
  • Option 007 required for CXA adjustments.

PSG3 Options UNR, UNX, or UNY

  • Option 1E1 required for CXA Option C75 Frequency Response test and adjustment.
  • Option 007 required for CXA adjustments.

A, P

Ultra Low Noise Source

Wenzel Associates Inc
Ultra Low Noise Reference Frequency Source:

  • Model 500-13438 Rev D
  • Rev D is required for DUTs with Option EP0.

Model 500-13438 Rev C

  • Rev C can be used as an alternate for all X-Series models EXCEPT for those with Option EP0. The performance of Rev C is insufficient for models with Option EP0.

P

Function Generator

33622A

33612A
33611A
33621A
33250A
33120A Option 001

  • Cannot be used for Option BBA, UXA > Option 526 adjustments, or any CXA Frequency Response Adjustments.

A, P

Analyzers

Spectrum Analyzer

  • Required for testing CXA Option T03/T06 only.

N9030B

N9030A
E4440A
E4445A
E4446A
E4448A

A, P

Network Analyzer

Used in adjustments for:

  • N9020B options > 526
  • N9021B all options
  • N9030B options > 526
  • N9040B options > 526

N5247B

  • Refer to the N7814A Readme for PNA firmware requirements.

N5247A/AS
N5245B
N5245A/AS

  • Refer to the N7814A Readme for PNA firmware requirements.

A, U

Audio Analyzer

  • Required for N9030B Option 107.

U8903B

Stanford Research Ultra Low Distortion Function Generator Model DS360

P

Counters

Universal Counter

53230A

53132A
53131A

A, P, T

Meters and Power Sensors
(See below for power sensor calibration service ordering guidelines.)

Digital Multimeter

3458A

34470A

A, P, T

Power Meter

N1914B

N1914A5, 7
N1912A

E4419A/B

  • Not allowed for the N9041B Total Amplitude Accuracy tests.

A, P, U

RF Power Sensor, Type-N (m) connector

  • 2 required

N8482A

N8482A CFT
8482A Option H84
8482A6

(Non-H84 sensors will increase measurement uncertainty.)

A, P

RF Power Sensor, Type-N (m) connector

  • 2 required
  • CXA only

E9304A Option H18

 

A, P

Microwave Power Sensor, 3.5 mm (m) connector

  • For N9030B and N9040B options > 526

E9304A Option H20

 

A

Microwave Power Sensor, 3.5 mm (m) connector

  • 2 required
  • For options ≤ 526

N8485A

N8485A CFT
8485A

 A, P

Millimeter Power Sensor, 2.4 mm (m) connector

  • 2 required
  • For options > 526

N8487A-CFT

N8487A
8487A

 A, P

Millimeter Power Sensor 3, 2.4 mm (m) connector

N8487A
(not for N9021B)

N8488A

 A, U

Millimeter Power Sensor 4, 1.85 mm (m) connector

N8488A

None

 A, U

Low Power Millimeter Power Sensor, 2.4 mm (m) connector

  • For options > 526

8487D

 

 A, P

Low Power Microwave Power Sensor, 3.5 mm (m) connector

  • 2 required
  • For Options P08, P13, or P26 only.

8485D

 

A, P

USB Power Sensor7, DC to 120 GHz, 1.0 mm (f) connector

  • For N9041B

U8489A Option 200

 

 P

75 Ω Power Sensor, Type-N (m) connector

  • For CXA Option C75 only.

8483A

 

P, A

Power Sensor Cable

  • 2 required

11730A

 

A, P, T

Standards

Frequency Standard

Microsemi 5071A-C002

HP/Agilent 5071A Option 001
Microsemi 5071A-C001

10 MHz External Reference8

A, P

50 MHz,
-
25 dBm Calibrator

Z5602B
   Opt H51 for Type-N models
   Opt H35 for 3.5 mm models
   Opt H24 for 2.4 mm models

Z5602A
   Opt H51 for Type-N models
   Opt H35 for 3.5 mm models
   Opt H24 for 2.4 mm models

A

Attenuators

10 dB
Step Attenuator9, 10

8496G Option 001, H50

8496H Option 001, H50

P

1 dB
Step Attenuator9, 10

8494G Option 001, H50

8494H Option 001, H50

P

Attenuator
Interconnect Kit

  • Type-N connector kit to connect the 8496G to the 8494G attenuator

11716A

 

 P

Attenuator Driver

11713D

11713E
11713B
11713A

 P

3 dB
Fixed Attenuator

8491A Option 003, H3311

8491B Option 003, H3311

P

6 dB
Fixed Attenuator

8490D Option 006

 

A, U

6 dB
Fixed Attenuator

8491A Option 006, H3311

8491B Option 006, H3311

P

6 dB
Fixed Attenuator

  • 2 required

8493C Option 006

 

A

10 dB
Fixed Attenuator

8491A Option 010, H3311

8491B Option 010, H3311

A, P

10 dB
Fixed Attenuator

8493C Option 010

 

A, P

10 dB
Fixed Attenuator, 2.4 mm (f) to 2.4 mm (m)

  • For N9030A/B and N9040B options > 526, and N9010N

8490D Option 010

 

P

20 dB
Fixed Attenuator

8491A Option 020

8491B Option 020

A, P

20 dB
Fixed Attenuator

  • For Option EXM only

8493C Option 020

 

P

30 dB
Fixed Attenuator

  • For use with low-power power sensors

11708A

 

A,P

30 dB
Fixed Attenuator, V-Band, waveguide

  • For N9041B

Sage Millimeter STA-30-15-F2

 

P

20 dB
Fixed Attenuator, W-Band, waveguide

  • For N9041B

Sage Millimeter STA-20-10-F2

 

P

Terminations

Type-N (m)

  • For Option 503, 508, 513

909A Option 012

 

P, T

3.5 mm (f)

  • For Option 526

909D

 

P, T

2.4 mm (f)

  • For options > 526

85138B

901D

A, P, T

BNC (m)

1250-0207

11593A

A, P, T

Miscellaneous Devices

RF Power Splitter, Type-N (f) connector

11667A

 

A, P

Microwave
Power Splitter, 3.5 mm (f) connector

11667B

 

A, P

Millimeter
Power Splitter, 2.4 mm (f) connector

  • For Options > 526

11667C

 

A, P

Directional Bridge, Type-N (f) connector

86205A

 

P

Directional Coupler, SMA (f) connector

87300C

 

P

Millimeter Directional Coupler, 2.4 mm (f) connector

  • For N9020B, N9030A/B, and and N9040B options > 526, and N9010N

87301C

 

P

Microwave
Power Divider, 3.5 mm(f) connector

11636B

 

A, P

Hybrid Power Divider, 3.5 mm (f) connector

87302C

 

A

Comb Generator

U9391G Option FFM

 

A, U

DC Power Supply

U8001A

 

A, U

mmWave Signal Generator Frequency Extender,
50 to 75 GHz

  • For N9041B

E8257DV15

 

P

mmWave Signal Generator Frequency Extender,
75 to 110 GHz

  • For N9041B

E8257DV10

 

P

Minimum Loss Pad
(50 Ω to 75 Ω), Type-N (f) to Type-N (m) connector

  • For CXA Option C75 only

11852B Option 401

 

A, P

ECal module, 2.4 mm, 50 GHz

N4693D Option M0F

N4693A Option M0F (N4693-60001)
N4693-61001

U

Cables

3.5 mm (m) to 3.5 mm (m) coaxial cable

  • 2 required
  • For Options ≤ 526

11500E

8120-4921

A, P

3.5 mm (m) to 3.5 mm (m) coaxial cable

11500F

 

A, P

2.4 mm (f) to 2.4 mm (m) cable

  • For Options > 526

8120-6164

 

A, P

2.4 mm (f) to 2.4 mm (m) cable

  • For Options > 526

8121-2065 (or equivalent)

 

A, P

1 mm (f) to 1 mm (m) cable

  • For N9041B

11500J

 

P

Type-N, Precision Type-N (m) both ends

  • 2 required

11500C

11500B

  • For CXA Option C75 only

A, P, T

Type-N, Precision Type-N (m) both ends

  • For CXA only

N6314A

 

A

BNC, 50 Ω Coax BNC (m) both ends

  • 3 required

8120-1840

8120-2582
10503A

A, P, T

Cable Assembly, banana plugs

U9391-20013

 

A, U

Filters

50 MHz Low Pass, BNC (m) to BNC (f)

  • Not required for EXA

Telonic Berkeley TLA 50-5AB2

0955-0306

P, T

300 MHz Low Pass, BNC (m) to BNC (f)

  • 2 required

Telonic Berkeley TLP 300-4AB4

0955-0455

P

1.8 GHz Low Pass, SMA (f) to SMA (f)

  • 2 required

RLC L-1636

0955-0491

P

5.0 GHz Low Pass, SMA (f) to SMA (f)

RLC F-30-5000-RF

 

P

8.0 GHz Low Pass, SMA (f) to SMA (f)

RLC F-30-8000-RF

 

P

12.4 GHz Low Pass, SMA (f) to SMA (f)

RLC F-30-12.4-RF

 

P

1 GHz Notch Filter

  • Not required if using the Wenzel source in the Phase Noise test.

Trilithic CFN-2-1000.1

 

P

Adapters

Type-N (f) to Type-N (f)

1250-1472

 

P

Type-N (m) to Type-N (m)

1250-1475

 

P

Type-N (m) (50 Ω) to Type-N (f) (75 Ω)

  • For CXA Option C75 only

1250-0597

 

A, P

Type-N (f) (75 Ω) to Type-N (f) (75 Ω)

  • For CXA Option C75 only

Huber + Suhner 31_N-75-0-2 /133_NE
(Item no. 22542612)

 

A, P

Type-N (f) to BNC (m)

1250-1477

 

P, T

Type-N (m) to BNC (m)

1250-1473

 

P, T

Type-N (m) to BNC (f)

1250-1476

 

P

Type-N (m) to 3.5 mm (m)

1250-1743

 

 

Type-N (m) to 3.5 mm (f)

  • 2 required

1250-1744

 

 

Type-N (f) to 3.5 mm (f)

  • For 3.5 mm source

1250-1745

 

 

Type-N (f) to 3.5 mm (m)

1250-1750

 

 

3.5 mm (f) to 3.5mm (f)

  • For 3.5 mm source

83059B

1250-1749

P

3.5 mm (m) to 3.5 mm (m)

  • 2 required

83059A

1250-1748

P

3.5 mm (m) to 3.5 mm (f)

83059C

 

P

3.5 mm (f) to 2.4 mm (f)

  • For 2.4 mm source

11901B

 

 

2.4 mm (f) to 2.4 mm (f)

  • For Options 543, 544, or 550

11900B

 

P

2.4 mm (f) to 3.5 mm (m)

11901D

 

A, P

2.4 mm (m) to 3.5 mm (f)

11901C

 

A

Type-N (f) to 2.4 mm (f)

  • For 2.4 mm source

11903B

 

A, P

Type-N (f) to 2.4 mm (m)

  • For N9041B

11903C

 

P

Type-N (m) to 2.4 mm (f)

  • For 2.4 mm source

11903D

 

P

2.4 mm (f) to 2.92 mm (f)

  • For N9010N

11904B

 

P, A

2.4 mm (m) to 2.92 mm (f)

  • For N9010N

11904C

 

P, A

2.4 mm (m) Aeroflex Weinschel Crown

  • For N9010N

7005A-13

 

P, A

1 mm ruggedized (f) to 2.4 mm (f) adapter

  • For N9041B

5067-6655

 

P

W-Band Waveguide to 1 mm adapter

  • For N9041B

Sage Millimeter SWC-101F-E1

 

P

V-Band Waveguide to 1 mm adapter

  • For N9041B

Sage Millimeter SWC-151F-E1

 

P

BNC (m) to SMA (f)

1250-1700

 

P

BNC Tee (BNC f,m,f)

1250-0781

 

A, P

BNC (f) to SMA (m)

1250-1200

 

A, P

BNC (f) to Dual Banana

1251-2277

 

A, P

1 mm (f) to 2.4 mm (f) adapter

  • For N9041B
  • Used with the U8489A 1.0 mm power sensor for power sensor calibration

11922B

 

P

3.5 mm (f) to Type-N (m)

  • For power sensor calibration

08485-60005

 

A, P

2.4 mm (f) to Type-N (m)

  • For power sensor calibration

08487-60001

 

A, P

Type-N Tee

1250-0559

 

P

Optional Equipment

10 MHz Distribution Amplifier

Microsemi 5087B

5087A

A, P

Table Footnotes:

  1. Keysight, Agilent, or Hewlett-Packard model numbers unless otherwise noted.

  2. A = Adjustments, P = Performance Testing, T = Troubleshooting

  3. Supported PSG models:

    • One PSG with Option 567, 1EA/1EU, 1E1, 007, and [UNX or UNR or UNY] can be used as the Microwave Signal Generator #1, Low Noise Signal Generator, and the RF Signal Generator.

    • PSG Option 521 is not supported as an alternative model for the X-Series performance verification tests due to its upper and lower frequency limits.

  4. The (obsolete) 836xxA/B/L synthesized generators are only allowed in the following applications:

    Mapped As

    Performance
    Verification

    Adjustments Utilities

    Signal Generator
    MW #1

    No

    Yes

    No

    Signal Generator
    MW #2

    Yes

    Yes

    No

     

  5. N1914A power meters with serial number prefix prior to MY53040007 require Service Note N1914A-07 which fixes a power supply ground loop. The ground loop injects noise into the measurement circuits which can cause unstable measurements at low (-30 dBm) power levels.

  6. The 8482A power sensor uses cal factors to compensate the power sensor for frequency response errors. Cal factors are stated in percentages. The 8482A factory cal factor uncertainty ranges from 2.2% to 3.1%. The cal factor uncertainty can be reduced to < 1.0% by using metrology grade calibration techniques. The power sensor cal factor uncertainty becomes one component of the Verification Test uncertainty analysis. Lower cal factor uncertainties will translate to wider test margins.

  7. The table below shows the various options that will provide USB ports on the N1914A power meter. Note that the N1914B power meter comes standard with USB ports.

     

  8. When using the 10 MHz External Reference (for performance tests), be sure to update the Additional Properties in TME to the correct Frequency Accuracy in parts per million (ppm). For example, if overall accuracy is 9e-12, the equivalent is 9e-6 ppm. Refer to the Additional Properties section in the N7800A TME Help for instructions.

  9. The step attenuators should be permanently joined using the 11716A Interconnect Kit as shown in the diagram.

     

  10. Step Attenuator Loss Characterization

    The step attenuator combination should have each attenuator setting characterized by a metrology lab at 50 MHz. This characterization can be ordered through Keysight Technologies as an Option H50 Calibration.

    The following tables show which sections of the 10 dB and 1 dB step attenuators are utilized for each attenuator setting. The tables also list the Recommended Uncertainty for each attenuator setting. A larger number will result in larger overall test uncertainties which could affect the test pass/fail rate.

    The interconnect cable should NEVER be disconnected once the loss characterization is performed.

    1 dB Step Attenuator

    Nominal Attenuation
    (dB)

    Attenuator Section

    Recommended Uncertainty
    (dB)

    #1

    (1 dB)

    #2

    (2 dB)

    #3

    (4 dB)

    #4

    (4 dB)

    0

    Off

    Off

    Off

    Off

    0 (Reference)

    1

    On

    Off

    Off

    Off

    < 0.005

    2

    Off

    On

    Off

    Off

    < 0.005

    3

    On

    On

    Off

    Off

    < 0.005

    4

    Off

    Off

    Ona

    Off

    < 0.005

    5

    On

    Off

    On

    Off

    < 0.005

    6

    Off

    On

    On

    Off

    < 0.005

    7

    On

    On

    On

    Off

    < 0.005

    8

    Off

    Off

    On

    On

    < 0.005

    9

    On

    Off

    On

    On

    < 0.005

    aTME requires that Section 3 be characterized.

     

    10 dB Step Attenuator

    Nominal Attenuation
    (dB)

    Attenuator Section

    Recommended Uncertainty
    (dB)

    #1

    (10 dB)

    #2

    (20 dB)

    #3

    (40 dB)

    #4

    (40 dB)

    0

    Off

    Off

    Off

    Off

    0 (Reference)

    10

    On

    Off

    Off

    Off

    < 0.010

    20

    Off

    On

    Off

    Off

    < 0.015

    30

    On

    On

    Off

    Off

    < 0.020

    40

    Off

    Off

    Ona

    Off

    < 0.025

    50

    On

    Off

    On

    Off

    < 0.030

    60

    Off

    On

    On

    Off

    < 0.035

    70

    On

    On

    On

    Off

    < 0.040

    aTME requires that Section 3 be characterized.

     

  11. 8491A Option H33 is a fixed attenuator which has been characterized to have a VSWR ≤ 1.05:1 at 50 MHz. A VSWR of 1.05:1 is recommended to test Input Attenuator Switching Uncertainty, Display Scale Fidelity, and Absolute Amplitude Accuracy performance tests. Any 8491A/B attenuator can be mapped into this device if the VSWR at 50 MHz has been characterized to be ≤ 1.05:1. When mapping the attenuator to indicate that it meets the required specification, the Option H33 checkbox will need to be checked in the configure test station Administration screen.

Guidelines for Ordering Power-Sensor Calibration Service

Use the following guidelines to ensure power sensors used by the N7800A application receive the correct calibration service:

  1. Order Option 1A7 when ordering new power sensors that will be used as working standards in N7800A TME calibrations.

  2. When ordering periodic calibration for instruments used as lab standards in the N7800A software, we recommend using “Keysight Cal + Uncertainties + Guardbanding”. More information can be found at http://www.keysight.com/find/americas_cal.

  3. The N7800A software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options (shown on the Special Calibrations Matrix located at http://cal.software.keysight.com) provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). The overall resulting N7800A measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N7800A calibration application are summarized in the Special Calibrations Matrix which can be found at http://cal.software.keysight.com.

  4. Option H99 is a special option for the Roseville Service Center [only] which provides electronic calibration data available as a .csv file that can be imported into TME thus avoiding manual entry. Option H99 must be requested from the Roseville Service Center upon re-calibration only of any previously purchased power sensor and not for new purchases of power sensors. This option may be ordered in addition to any other required or requested Std Lab Calibration option. Option H99 is recommended but not required.

    The following models are not supported by Option H99:

    • E9304A-H18, H19, H84
    • E9300A-H25
    • N8386A
    • N8486AQ

Calibration Data Validation

Standard Checks

To ensure data integrity for measurements carried out with TME (Test Management Environment), the following verification checks are carried out at the beginning of each test run. The checks are only performed on devices that require calibration data which directly affect the test results.

The following table lists the standard checks performed by default:

Failure to comply with the CalFactor(%) or Atten(dB) will result in test data being labeled Invalid in both the TME interface and in any report format produced from the data.

 

Device Parameter Name and Description Limits A Failure
Affects:

Noise Source

NoiseRatio(dB)
The extended noise ratio, in dB

Must be > 0 and ≤ 30 at all points

All test runs

Power Sensor

CalFactor(%)
The calibration factor, as a percentage

Must be ≥ 10% and ≤ 150% at all points.
Must not be 100% (the default) at all points.

All test runs

Uncertainty(%)
The uncertainty of the calibration factor, as a percentage

Must be > 0 and ≤ 10% at all points

Test runs guard banded by measurement uncertainty only

ReflectCoeff(Mag)
The magnitude of the reflection coefficient

Must be > 0 and < 0.5 at all points

Test runs guard banded by measurement uncertainty only

Power Sensor
(Wide Band)

LowBandCalFactor(%)
The calibration factor, as a percentage, for the low band

Same tests as for CalFactor(%) on a one-range power sensor

All test runs

HighBandCalFactor(%)
The calibration factor, as a percentage, for the high band

Same tests as for LowBandCalFactor(%)

All test runs

LowBandUncertainty(%)
The uncertainty of the calibration factor, as a percentage, for the low band

Same tests as for Uncertainty(%) on a one-range power sensor

Test runs guard banded by measurement uncertainty only

HighBandUncertainty(%)
The uncertainty of the calibration factor, as a percentage, for the high band

Same tests as for LowBandUncertainty(%)

Test runs guard banded by measurement uncertainty only

ReflectCoeff(Mag)
The magnitude of the reflection coefficient

Same tests as for ReflectCoeff(Mag) on a one-range power sensor

Test runs guard banded by measurement uncertainty only

Step Attenuator

Atten(dB)
The attenuation, in dB

Must be within 1 dB of the nominal attenuation.
Must not all be exactly equal to the nominal attenuation (the default) at all points except zero, zero step is the reference and must be zero

All test runs

Uncert(dB)
The uncertainty of the attenuation, in dB

Must be > 0 and ≤ 0.1 dB at all points except zero. Zero step is the reference and must be zero.

Test runs guard banded by measurement uncertainty only

ReflSize
The reflection coefficient magnitude

Must be > 0 and < 0.5 at all points

Test runs guard banded by measurement uncertainty only