NFA — N8973B/74B/75B/76B
This test measures the amplitude accuracy of the External Mixer Input. This test is performed by placing a 322.5 MHz signal of known amplitude into the signal analyzer. The signal analyzer is placed in External Mixing Mode, thus enabling the IF Input port, and the amplitude is measured on the signal analyzer. The difference between the measured amplitude and the known amplitude is called the External IF amplitude error. This error is compared to the specification and a Pass/Fail determination is made. The main source of measurement errors are generated from the power meter measurement.
The 20 dB attenuator presents a controlled match to the External Mixer port. The low pass filter is used to prevent the DUT's external LO signal from modulating the ALC loop in the signal source.
Click here for troubleshooting.
|
Test Equipment |
Recommended Model Number |
|---|---|
|
Synthesized Sweeper |
PSG Models |
|
Power meter |
N1914B |
|
RF power sensor |
N8485A |
|
20 dB reference attenuator |
8493C, Option 020 |
|
5.0 GHz Low Pass Filter |
RLC F-30-5000-RF |
|
Cable, 3.5 mm |
8120-4921 |
|
Cable, BNC |
8120-1840 |
|
3.5 mm (f) to 3.5 mm (f) adapter |
83059B |
|
Type-N (m) to 3.5 mm (f) adapter |
08485-60005 |
|
2.4 mm (f) to 3.5 mm (f) adapter |
11901B |