IF Input Gain Accuracy Option EXM Performance Test

This test applies to the following models with Option EXM:

This test measures the amplitude accuracy of the External Mixer Input. This test is performed by placing a 322.5 MHz signal of known amplitude into the signal analyzer. The signal analyzer is placed in External Mixing Mode, thus enabling the IF Input port, and the amplitude is measured on the signal analyzer. The difference between the measured amplitude and the known amplitude is called the External IF amplitude error. This error is compared to the specification and a Pass/Fail determination is made. The main source of measurement errors are generated from the power meter measurement.

The 20 dB attenuator presents a controlled match to the External Mixer port. The low pass filter is used to prevent the DUT's external LO signal from modulating the ALC loop in the signal source.

Click here for troubleshooting.

Required Test Equipment

Test Equipment

Recommended Model Number

Synthesized Sweeper

PSG Models
(see equipment list)

Power meter

N1914B

RF power sensor

N8485A

20 dB reference attenuator

8493C, Option 020

5.0 GHz Low Pass Filter

RLC F-30-5000-RF

Cable, 3.5 mm

8120-4921

Cable, BNC

8120-1840

3.5 mm (f) to 3.5 mm (f) adapter

83059B

Type-N (m) to 3.5 mm (f) adapter

08485-60005

2.4 mm (f) to 3.5 mm (f) adapter
(for 2.4 mm source)

11901B

Connection Setups

Power Meter Calibration

 

IF Input Gain Accuracy Calibration Setup

 

IF Input Gain Accuracy Test Setup