All X-Series models
This test evaluates the accuracy of the input step attenuator (electromechanical or electronic) at 50 MHz. A source is connected to the analyzer through a composite 10-dB-step and 1-dB-step precision attenuator. The external (reference) and internal (DUT) attenuators are stepped in opposite directions to maintain -81 dBm at the input mixer of the DUT. The DUT display is used to indicate the difference between the change in the internal attenuator and the change in the external composite precision attenuator. As the DUT attenuator is changed, the reference level is changed to keep the trace near the same position on the display.
|
This test requires step attenuator calibration data to obtain valid results. Make sure you enter the calibration data for the step attenuators that you're using. Please refer to the Enter Equipment Calibration Data section in the TME help for details on how to enter this data. You must enter the data for the following columns to obtain valid results: Attn(dB), Uncert(dB) and ReflSize. |
Click here for troubleshooting.
Test Equipment |
Recommended Model Number |
---|---|
Low Noise Signal Generator |
PSG Models |
1 dB Step Attenuator |
8494G Option 001, H50 |
10 dB Step Attenuator |
8496G Option 001, H50 |
Attenuator Driver |
11713B |
Attenuator Interconnect Kit |
11716A |
6 dB Fixed Attenuator |
8491A Option 006, H33 |
10 dB Fixed Attenuator |
8491A Option 010, H33 |
BNC Cable |
8120-1840 |
Type-N Cable |
11500C |
Viking Cable |
8120-2703 |
Type-N (f) to 2.4 mm (f) adapter |
11903B |
Type-N (f) to 3.5 mm (f) adapter |
1250-1745 |
|
In the following setups, cables are designated as solid lines and direct connections are designated as dashed lines. |