All X-Series models
This test verifies the analyzer Noise Sideband specification.
The test requires that DANL at 1 GHz be characterized for the near noise corrections. If the DANL test has been run, the DANL test data will be used. If DANL has not been run, then the DANL will be characterized at 1 GHz.
There are two solutions available for testing phase noise. The preferred solution is the Wenzel Ultra Low Noise source. The alternate solution is the PSG signal generator with a notch filter. Some X-Series models can only use the preferred solution as explained below.
For some X-Series models, only the Wenzel preferred solution is allowed because the PSG alternate solution cannot provide the phase noise performance required.
The following X-Series models can only use the Wenzel preferred solution. The alternate solution is not allowed.
UXA N9040B with Option EP0
The alternate solution uses a PSG signal generator as the source (Opt. UNX or UNR) with a 1.0001 GHz notch filter which will reduce the source phase noise at offsets above 100 kHz. The analyzer center frequency is tuned such that the offset frequency is centered in the notch. The notch filters out approximately 5 dB of noise contribution that the source creates. The notch bandwidth is very narrow, so the analyzer Resolution Bandwidth must be kept narrow (1 kHz) in order to prevent out-of-band noise from entering the measurement.
Click here for troubleshooting.
Test Equipment |
Model Number |
---|---|
Preferred Solution1 |
|
Ultra Low Noise Signal Source |
Recommended model:
Alternative model for all X-Series analyzers EXCEPT for DUTs with Option EP0:2
|
Alternate Solution3 |
|
RF Signal Generator |
PSG Models |
1 GHz Notch Filter |
Trilithic CFN-2-1000.1 |
Miscellaneous Devices |
|
50 ohm Termination |
909A, Option 012 |
2.4 mm (f) Termination |
85138B |
3.5 mm (f) Termination |
909D |
BNC Cable |
8120-1840 |
Coaxial Cable, 3.5 mm |
11500E |
3.5 mm (f) to 3.5 mm (f) adapter |
83059B |
Type-N (m) to 3.5 mm (f) adapter |
1250-1744 |
2.4 mm (f) to 3.5 mm (f) adapter |
11901B |
|
|
In the following setups, cables are designated as solid lines and direct connections are designated as dashed lines. |