N9038B MXE
The EMI receiver Overload Detector is adjusted by inputting a known signal level and adjusting the Overload DAC until the Overload Indicator is tripped. The DAC value is then stored in memory.
The EMI receiver RF Preselector is comprised of 23 unique signal paths. Each path will have its own unique Overload DAC setting. The Overload Detector DAC value will be determined for 16 paths. Some of the wider filter segments have multiple DAC values. Some paths will have the DAC defaulted to 255 (the maximum value). The Overload DAC is an 8-bit DAC.
You may get a GPIB connection error when using the IGUU 2918.
There is a known issue with certain versions of the Keysight IO Library not recognizing the Schwarzbeck IGUU 2918 pulse generator and therefore causing a GPIB connection failure. There are two work-around methods to correct this error. Refer to the Connecting GPIB Instruments section of Getting Started for more information.
|
Test Equipment |
Recommended Model Number |
Alternative Model Number |
|---|---|---|
|
DC Pulse Generator |
Schwarzbeck IGUU 29181 |
Schwarzbeck IGUU 29161 |
|
Cable, Type-N |
11500C |
|
|
Adapter, Type-N (f) to 3.5 mm (f)
|
1250-1745 |
|
|
Adapter, Type-N (f) to 2.4 mm (f)
|
11903B |
|
Click on the links below for images depending on the pulse generator model being used.