This test verifies that the signal generator provides a functional CW signal with the RF path below 3.2 GHz set to Wide IQ/FM. Maximum output power with Wide IQ/FM On (called Wide FM/fM for Option HTS) is described as a nominal specification. Generally nominal parameters are not tested. Maximum output power with Wide IQ/FM ON is tested because there is a minimum level of functionality that needs to be guaranteed.
During this test, the signal generator is set to its maximum settable output power and a measurement is performed using a power meter. The measured power is compared against a limit that verifies functionality.
|
Test Equipment |
Recommended Models |
Alternate Model(s) |
|
Power Meter |
N1914A1 |
E4419A/B (with firmware A2.09.01 or greater when using N-Series sensors) |
|
Power Sensor (Low Frequency) |
E9304A H192 |
E9304A |
|
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this performance test, follow all instructions on the controller display.
This test uses flexible power sensor channel assignment and will identify the channel that a power sensor is connected to using the ability of "smart" sensors such as the N848xA, U848xA, and E930xA series to report their full model and serial number. Legacy 848x series power sensors are unable to provide their model or serial number, but their channel is identified during the sensor calibration process by identifying the channel of the sensor connected to the calibrator.
If the wrong legacy power sensor is connected to the calibrator during this process, the error can be resolved by disconnecting and reconnecting the power sensor to the power meter which will force a new calibration.
Select from the links below for connection setups depending on the power sensor selection. To expand all, click the Expand All button
in the toolbar (webhelp only).
Power sensor calibration — standard sensor
Measurement setup — standard sensor channel A
Measurement setup — standard sensor channel B
Power sensor calibration — USB sensors
Measurement setup — USB sensor channel C
Measurement setup — USB sensor channel D
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the Performance Test.
If this test fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.