This section lists the test equipment needed to run performance tests, adjustments, and utilities. Any critical specification requirements are noted, as well as recommended model numbers. Refer to each individual test for specific setup configurations with required cables and adapters. The computer and all test equipment are connected to the DUT using GPIB. All test equipment is Keysight (previously Hewlett-Packard and Agilent) unless otherwise noted.
|
|
In all test equipment configurations, cables and adapters must be properly torqued. Exceeding recommended torque values can cause damage to a cable or adapter, and can cause inaccurate test results. |
|
|
|
|
Test Equipment |
Recommended Models |
Alternate Models |
Applicable Tests/Comments |
|
Sources |
|||
|
External Baseband
|
N5182B Opt 656 or 657 |
N5182A Opt 651, 652, or 654 E4438C Opt 402 and [001, 002, 601, or 602] |
|
|
Phase Noise Reference Source |
E8257D Opt UNT, UNY, 1EU
E8257D Opt HY21
E8663D Opt HY21
|
E8257D Opt UNT, UNX1 or HNY4, 1EU E8247C Opt UNR2 E8663D Opt UNT, UNX1 or UNY, 1EU 8662A2, 3
|
|
|
Function Generator |
33622A |
33611A |
Maximum Output Power - Digital Mode External Frequency Modulation Frequency Response External Pulse Modulation On/Off Ratio External FM Deviation Accuracy |
|
Analyzers |
|||
|
Network Analyzer
|
N5245B |
N5222A/B1, N5224A/B, N5225A/B, or N5227A/B N5232A/B1, N5234A/B, or N5235A/B N5242A/B1, N5244A/B, N5245A, or N5247A/B E8361A/C N5230A/C Opt 2201, 2251, 2401, 2451, 2461, 420, 425, 520, or 525
|
|
|
N9030B Opt 5501, MPB2, Pxx3, YAV4, and N9063EM0E Analog Demodulation Measurement application5, 6
|
N9030A Opt 5501, MPB2, Pxx3, YAV4, and N9063EM0E Analog Demodulation Measurement application5, 6, 7
E444xA1 Opt 1102, 1233, 1244, 2335
|
Internal FM Frequency Response Internal Phase Modulation Deviation Accuracy Internal Phase Modulation Distortion Amplitude Modulation Distortion Frequency Modulation Residual FM Frequency Modulation Incidental AM Amplitude Modulation Depth Accuracy External Frequency Modulation Frequency Response Scan Modulation Rise/Fall Time External Pulse Modulation On/Off Ratio |
|
|
Vector Signal Analyzer
|
89441A Opt AYA, AYH, AY9, and UFG or UTH |
|
|
|
Vector Signal Analysis Application
|
89600 VSA with these options:
NOTES:
|
|
|
|
Measuring Receiver
|
8902A
|
|
Internal FM Frequency Response Internal Phase Modulation Deviation Accuracy Internal Phase Modulation Distortion |
|
Audio Analyzer
|
8903A
|
|
|
|
Meters and Power Sensors (See below for power sensor calibration ordering guidelines.) |
|||
|
Digital Voltmeter |
3458A Opt 002 |
34470A
|
Maximum Output Power - Digital Mode External Frequency Modulation Frequency Response External FM Deviation Accuracy |
|
Power Meter |
N1914A1
|
E4419B1
|
Maximum Output Power - Digital Mode |
|
Power Sensor (Low Frequency) |
E9304A H191
|
E9304A1,2,
|
Maximum Output Power - Digital Mode Maximum Output Power - Wide IQ/FM Mode
|
|
Power Sensor (Mid Frequency)
|
N8487A1
|
8487A H841, 2
|
Maximum Output Power - Digital Mode1 Digital Modulation Power Relative to CW2, 3
|
|
Power Sensor (High Frequency)
|
V8486A H671,2,3
|
N8488A
|
|
|
Coaxial to V Band Adapter
|
V281A1
|
|
|
|
Attenuators |
|||
|
3 dB Attenuator
|
8490D Opt 003 |
8491x Opt 003 |
|
|
6 dB Attenuator
|
8490D Opt 006 |
8491x Opt 006 |
|
|
10 dB Attenuator
|
8490D Opt 010 |
8493C Opt 010
|
Internal Pulse Modulation Level Accuracy |
|
20 dB Attenuator
|
8493C Opt 020 |
|
Internal Pulse Modulation Level Accuracy |
|
Oscilloscopes |
|||
|
Oscilloscope |
DSOS104A Opt 100, 200, or 4001,2
|
54810A1, 2 DSO8064A Opt 6403 MSO8064A Opt 6403
|
|
|
Oscilloscope Mainframe |
N1000A |
86100D 86100A (with firmware A.02.10 or greater) |
Internal Pulse Modulation Level Accuracy |
|
Oscilloscope Plug-In |
N1045B1
|
N1045A1 86117A/B
|
Internal Pulse Modulation Level Accuracy |
|
Local Oscillator
|
E8257D Opt (550 or 567) and (1EA or 1EU) and (UNR, UNX, UNY, or HNY) |
For PSG-D with Opt 520,
E8257D Opt (520 or 540) and (1EA or 1EU) and (UNR, UNX, UNY, or HNY) E8257D Opt 521 and (UNX, UNY, or HNY) E8267D Opt 520 and (UNR, UNX or UNY) E8241A Opt 1EA and UNJ E8244A Opt 1EA and UNJ E8251A Opt 1EA and UNJ E8254A Opt 1EA and UNJ E8247C Opt 1EA and UNR E8257C Opt 1EA and UNR E8267C Opt UNR
For PSG-D with Opt 532,
E8257D Opt 540 and (1EA or 1EU) and (UNR, UNX, UNY, or HNY) E82x4A Opt 1EA and UNJ E8247C Opt 540 and 1EA and UNR E8257C Opt 540 and 1EA and UNR |
|
|
Mixers |
|||
|
Mixer
|
0955-2225 |
0955-1017 |
|
|
Mixer
|
Marki M4-0265 |
|
|
|
Calibration Kits |
|||
|
2.4 mm Calibration Kit
|
N4693D Option M0F (E-Cal Kit) |
N4693-60001 (E-Cal Kit) 85056A1 (Mechanical Cal Kit)
|
|
|
3.5 mm Calibration Kit
|
N4691D Option M0F (E-Cal Kit) |
N4691-60004 (E-Cal Kit) 85052B1/D (Mechanical Cal Kit)
|
|
|
Miscellaneous Devices |
|||
|
Frequency Counter |
53230A Opt (106 or 115)1
|
53132A Opt (050 or 124)1 53132A Opt (050 or 124)1 and Opt (001, 010, or 012)2
|
|
|
Frequency Standard |
Microsemi 5071A |
|
|
|
Phase Noise System |
N5511A Options 540, CH21
|
E5505A Option 001
|
|
|
Power Splitter
|
Mini-Circuits ZFSC-2-2-S+ (Keysight part number 0955-2274) |
|
|
|
Diode Detector
|
33330C |
|
|
|
2.4 mm (male) Aeroflex Weinschel Crown
|
7005A-13 |
|
All |
To use the PXA N9030A with N9063EM0E analog demodulation measurement application functionality above 3.5 GHz or for modulation rates above 50 kHz, the N9030A must be upgraded with one of the following upgrade options: MTU or TES. After either upgrade, the N9030A must be re-calibrated for analog demodulation specifications above 3.5 GHz to be valid.
Choose from one of the following options:
Option MTU — Multi-Touch User Interface
For analog demodulation specifications above 3.5 GHz to be valid, Option MTU can only be installed on N9030A instruments with serial number prefix greater than or equal to MY/SG/US5449.
Option TES — TOI Enhanced Specifications
Option TES is a Keysight-only internal option. Keysight service centers need to contact the CSG support node to obtain an internal license key for this option.
USB power sensors require a power meter with USB ports. The table below shows the various options that will provide USB ports on the TME recommended N1914A power meter.
|
N1914A Orderable Options |
Description |
FW responds as option1 |
|
|
201 |
Ordered from the factory with new N1914A |
Dual channel average power meter with VGA, trigger in/out, 1 front and 1 rear USB port |
008, 010, 012 |
|
The following options are ordered as upgrades to an existing N1914A power meter. |
|||
|
106 |
This is the recommended option. |
Dual channel average power meter with 1 front and 1 rear USB port |
008 |
|
103 |
alternate |
Dual channel average power meter, battery, 2 rear USB ports |
001, 009 |
|
105 |
alternate |
Dual channel average power meter with VGA, battery, 1 front and 1 rear USB port |
008, 010 |
|
108 |
alternate |
Parallel rear-panel sensor input connectors, front-panel reference calibrator connector, 2 rear USB ports |
002, 009 |
|
109 |
alternate |
Parallel rear-panel sensor input connectors, rear-panel reference calibrator connector, 2 rear USB ports |
003, 009 |
|
111 |
alternate |
Dual channel average power meter, battery, 1 front and 1 rear USB port |
001, 008 |
|
167 |
alternate |
Dual channel average power meter, external trigger in/out, 1 front and 1 rear USB port |
008, 012 |
|
|
Test Equipment |
Recommended Model |
Alternate Models |
|
|
Sources |
|||
|
PSG/ESG Signal Generator |
E4438C ESG Vector signal generator with Options 001 or 002 or 601or 602 |
E8267C PSG Vector signal generator with Options 002, 602 E8267D PSG Vector signal generator with Options 601, 602 |
|
|
Function Generator |
33250A |
33120A Opt 001 |
|
|
Analyzers |
|||
|
Spectrum Analyzer |
E444xA1 Opt 233
|
|
|
|
Power Meters and Sensors (See below for power sensor calibration ordering guidelines.) |
|||
|
Power Sensor (Low Frequency) |
E9304A H19 |
E9304A
|
|
|
Power Sensor (Mid Frequency) |
N8487A |
N8485A
|
|
|
Power Sensor (High Frequency) |
V8486A |
|
|
|
Power Meter |
N1914A1
|
E4419A |
|
|
Digital Multimeter |
3458A Option 002 |
|
|
|
Attenuators |
|||
|
Attenuator |
8490D Opt 010 |
8493C Opt 010 |
|
|
Oscilloscopes |
|||
|
High Frequency Oscilloscope Mainframe |
86100D |
54750A |
|
|
Oscilloscope Plug-In |
86117A |
86117B |
|
|
Miscellaneous Devices |
|||
|
Frequency Counter |
53230A Opt 1061 or 1151
|
53132A Opt 050 or 124 |
|
|
Coaxial to V Band Adapter |
V281A |
Used with V8486A power sensor |
|
|
2.4 mm (male) Aeroflex Weinschel Crown
|
7005A-13 |
|
|
|
Test Equipment |
Recommended Model |
Alternate Models |
|
Frequency Counter |
53230A Opt 1061 or 1151
|
53132A Option 0501 or 1241
|
|
Frequency Standard |
10 MHz house standard |
For example, a Microsemi 5071A primary frequency standard or equivalent can be used. |
|
2.4 mm (male) Aeroflex Weinschel Crown
|
7005A-13 |
|
Order Option 1A7 when ordering new power sensors that will be used as working standards in N78xxxB ETMS calibrations.
When ordering periodic calibration for instruments used as lab standards in N78xxxB ETMS software, we recommend using “Keysight Cal + Uncertainties + Guardbanding”. More information can be found at http://www.keysight.com/find/americas_cal.
The N7800A software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options (shown on the Special Calibrations Matrix located at http://cal.software.keysight.com) provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). The overall resulting N78xxxB measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N78xxxB ETMS calibration application are summarized in the Special Calibrations Matrix which can be found at http://cal.software.keysight.com.
Option H99 is a special option for the Roseville Service Center [only] which provides electronic calibration data available as a .csv file that can be imported into TME thus avoiding manual entry. Option H99 must be requested from the Roseville Service Center upon re-calibration only of any previously purchased power sensor and not for new purchases of power sensors. This option may be ordered in addition to any other required or requested Std Lab Calibration option. Option H99 is recommended but not required.
|
|
The following models are not supported by Option H99:
|