|
|
The ALC Conditioning Calibration and Absolute Power Calibration must be run prior to this adjustment. |
This adjustment calibrates the accuracy of the leveling control. There are three functions called for each frequency which fill the arrays associated with this calibration:
fillLevelArray
measurePowerAtDacSettings
interpolateArray
|
Test Equipment |
Recommended Model |
Alternate Model(s) |
|
Spectrum Analyzer |
PXA N9030B Options MPB, Pxx1 |
PXA N9030A Options MPB, Pxx1 PSA models Options 123, [1DS or 110]1: |
|
|
|
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
Refer to the troubleshooting section of the service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight website.
If necessary, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.